This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

双电机快速电流环程序SpeedRef 设置问题



 motor1.SpeedRef = MOTOR1_FORCE_ANGLE_SPEED;  //0.05;
#define  MOTOR1_FORCE_ANGLE_SPEED  0.0125*MOTOR1_RATED_SPEED
#define  MOTOR1_RATED_SPEED        (MOTOR1_RATED_FREQ / MOTOR1_BASE_FREQ)
#define MOTOR1_RATED_FREQ     400.0       // Rated motor electrical freq
#define MOTOR1_BASE_FREQ      500.0       // Base electrical frequency (Hz) -for inverter

在双电机快速电流环程序中关于SpeedRef的设置没看懂 其中0.0125*MOTOR1_RATED_SPEED中的0.0125不知道怎么来的,还有MOTOR1_RATED_FREQ / MOTOR1_BASE_FREQ不知道干嘛用的,是用来标幺化?

  • “在双电机快速电流环程序中关于SpeedRef的设置没看懂 其中0.0125*MOTOR1_RATED_SPEED中的0.0125不知道怎么来的,还有MOTOR1_RATED_FREQ / MOTOR1_BASE_FREQ不知道干嘛用的,是用来标幺化?”
    Eric:
    0.0125这个是TI自己根据经验设置的吧,一般也就是几HZ,像InstaSPIN算法里面是用到了2Hz.
    MOTOR1_RATED_FREQ / MOTOR1_BASE_FREQ 这个是计算标幺化的。