This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Flash28_API:
{
-l F021_API_F28004x_FPU32.lib
}
LOAD = FLASHB,
RUN = RAMGS7,
LOAD_START(_Flash28_API_LoadStart),
LOAD_SIZE(_Flash28_API_LoadSize),
LOAD_END(_Flash28_API_LoadEnd),
RUN_START(_Flash28_API_RunStart),
RUN_SIZE(_Flash28_API_RunSize),
RUN_END(_Flash28_API_RunEnd),
PAGE = 0, ALIGN(4)
编译结果:Description Resource Path Location Type
#10068-D no matching section 280049_FLASH_lnk.cmd /TBM14_3200SI line 327 C/C++ Problem指向的是 -l F021_API_F28004x_FPU32.lib位置。我在属性-C2000 linker-file serach path里已经添加过了F021_API_F28004x_FPU32.lib文件。导致我现在调用的FLASHAPI 函数都报未定义的错误。
上述内存的flash和ram的分配已经在TMS320F28075上验证过没问题的。