This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28034 的I2C 控制AT24C08 异常问题?



AT24C08 的A0、A1、A2、WP引脚接GND

#define EEPROM_SLAVE_ADDR      (0xA0 >> 1) (p0 p1=00 :默认访问第一块)

void Init_I2c(void)

{
 GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;    // Enable pull-up for GPIO32 (SDAA)
 GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0;    // Enable pull-up for GPIO33 (SCLA)
 GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 3;  // Asynch input GPIO32 (SDAA)
    GpioCtrlRegs.GPBQSEL1.bit.GPIO33 = 3;  // Asynch input GPIO33 (SCLA)
 GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1;   // Configure GPIO32 for SDAA operation
 GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1;   // Configure GPIO33 for SCLA operation

    // Initialize I2C
    I2caRegs.I2CMDR.all = 0;//I2C reset

    I2caRegs.I2CPSC.all = 5;      // Prescaler - need 7-12 Mhz on module clk 60Mhz/(5+1)=10mhz 系统时钟60M,使用内部时钟1
    //400khz=clk  10mhz/((clkL+5)+(clkH+5))
//    I2caRegs.I2CCLKL = 10;   // NOTE: must be non zero
//    I2caRegs.I2CCLKH = 5;   // NOTE: must be non zero
    //clk=100khz
    I2caRegs.I2CCLKL = 50;   // NOTE: must be non zero
    I2caRegs.I2CCLKH = 40;   // NOTE: must be non zero

   // I2caRegs.I2CIER.all = 0x24;  // Enable SCD & ARDY __interrupts
    I2caRegs.I2CIER.all = 0x00;  // no __interrupts

    I2caRegs.I2CMDR.bit.IRS = 1;//I2C enable    是不是时钟使能后 SCL线上就能测试到时钟波形了,还是发送启动信号后才能测试到?
    I2caRegs.I2CMDR.bit.FREE = 1;//interrupt 不影响接收发送
    I2caRegs.I2CFFTX.all = 0x6040; // Enable FIFO mode and TXFIFO
    I2caRegs.I2CFFRX.all = 0x2044; // Enable RXFIFO, clear RXFFINT,
    /*
     * 1、I2CSAR 在初始化时没必要配置,用到那个从设置,就设置这个值,写入的地址等于实际的地址左移一位的值,目的是把读写位去掉
     * 2、I2C模块的操作采用FIFO查询的方式进行
     */
}

curr_Msg.MsgStatus = I2C_MSGSTAT_SEND_WITHSTOP;
   curr_Msg.SlaveAddress = EEPROM_SLAVE_ADDR;
  // curr_Msg.MemoryHighAddr = paramData[1];
   curr_Msg.MemoryLowAddr = paramData[2];
   curr_Msg.NumOfBytes =1;
   curr_Msg.MsgBuffer[0] = paramData[4];
   I2CA_WriteData(&curr_Msg);//调用任意地址写函数


Uint16 I2CA_WriteData( struct I2CMSG* msg)
{
   Uint16 i;

   // Wait until the STP bit is cleared from any previous master communication.
   // Clearing of this bit by the module is delayed until after the SCD bit is
   // set. If this bit is not checked prior to initiating a new message, the
   // I2C could get confused.
   if (I2caRegs.I2CMDR.bit.STP == 1)
   {
      return I2C_STP_NOT_READY_ERROR;
   }

   // Setup slave address
   I2caRegs.I2CSAR = msg->SlaveAddress;

   // Check if bus busy
   if (I2caRegs.I2CSTR.bit.BB == 1)
   {
      return I2C_BUS_BUSY_ERROR;
   }

   // Setup number of bytes to send
   // MsgBuffer + Address

    I2caRegs.I2CCNT = msg->NumOfBytes+1;
 //   I2caRegs.I2CDXR = msg->MemoryHighAddr;
   // Setup data to send
   I2caRegs.I2CDXR = msg->MemoryLowAddr;

   for (i=0; i<msg->NumOfBytes; i++)
   {
      I2caRegs.I2CDXR = *(msg->MsgBuffer+i);
   }
   I2caRegs.I2CFFTX.bit.TXFFINTCLR =1;
   /*
    * 清楚标志位,一定要写完数据在清楚,不然清楚不了,因为IL的值设置的为0
    */
   // Send start as master transmitter
   I2caRegs.I2CMDR.all = 0x6E20;// 这里执行后,SDL和SDA 两根线上无波出来,一直都是高电平
//   I2caRegs.I2CMDR.bit.MST =1;
//   I2caRegs.I2CMDR.bit.TRX=1;
//   I2caRegs.I2CMDR.bit.STT =1;
//   I2caRegs.I2CMDR.bit.STP =1;
   /* bit15:NACKMOD=0 receive 时才有用,发送模式无用
    * bit14:FREE=1: 在调试模式下,模块不受断点影响,可以正常工作
    * bit13:STT =1  :在主模式下,产生一个起始信号
    *
    * bit11:STP =1  :内部计数器减为0时,产生一个stop信号
    * bit10:MST =1  :模块工作在主模式
    * bit9 :TRX =1  :transmitter mode
    * bit8 :XA  =0  :7bit address mode
    *
    * bit7: RM  =0  : NonRepeat mode
    * bit6: DLB = 0  :Digital loopback mode is diaable
    * bit5: IRS = 1;   The I2C module is enabled
    * bit4: STN = 0: The I2C module is not in the START byte mode
    *
    * bit3: FDF = 0:  Free data format mode is disable ,地址位是7位或10位
    * bit2~0: BC = 0;8 bit per data Byte
    *
    */
   while(I2caRegs.I2CFFTX.bit.TXFFST !=0){}//等待数据发送完成    程序死在这里,也就是说TXFFST的位等于写入的数据个数,这里为2.这个程序是在377XD

//系列上调试过的没有什么问题,只是更改了一个EEPROM内部写入的地址,望指点
   if(I2caRegs.I2CSTR.bit.SCD == 1)
 I2caRegs.I2CSTR.bit.SCD = 1;
/*
 * SCD=1 清楚SCD 和NACK位
 */

   return I2C_SUCCESS;
}

  • // 回环测试 start
    I2caRegs.I2CMDR.bit.MST=1;
    I2caRegs.I2CMDR.bit.TRX=1;
    I2caRegs.I2CMDR.bit.DLB =1;
    while(!(I2caRegs.I2CSTR.bit.XRDY ==1));
    I2caRegs.I2CDXR = 0xaa;
    I2caRegs.I2CMDR.bit.STT =1;
    data = I2caRegs.I2CDRR;
    while(!(I2caRegs.I2CSTR.bit.XRDY ==1));
    I2caRegs.I2CDXR = 0x55;
    data = I2caRegs.I2CDRR;
    I2caRegs.I2CMDR.bit.STP =1;
    //end
    验证了一下回环的功能,也是OK的 I2CDRR 中的数据等于I2cDXR 中的数据。