This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C28346的外部ADC时钟信号如何产生?



怎么配置寄存器可以使EXTADCCLK引脚输出时钟信号

  • 您可以看一下 www.ti.com/.../sprufn1c.pdf 的 Table 6. High-Speed Peripheral Clock Prescaler (HISPCP) Field Descriptions

    其中HSPCLK

    These bits configure the high speed peripheral clock rate with reference to SYSCLKOUT and the clock output of this prescaler is used in generating the SOCs and the external ADC clock (EXTADCCLK), used for external ADC interface. At reset, the EXTADCCLK will be generated and sent out so that external ADCs that need a clock at reset can work properly. HSPCLK = SYSCLKOUT / [(HISPCP +1)* 2]