This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28027的I2C模块



手册中未给出配置使用步骤,例程中有I2C和EEPROM的通信,在历程中看到发数据是这样的过程

Uint16 I2CA_WriteData(struct I2CMSG *msg)
{
   Uint16 i;

   // Wait until the STP bit is cleared from any previous master communication.
   // Clearing of this bit by the module is delayed until after the SCD bit is
   // set. If this bit is not checked prior to initiating a new message, the
   // I2C could get confused.
   if (I2caRegs.I2CMDR.bit.STP == 1)
   {
      return I2C_STP_NOT_READY_ERROR;
   }

   // Setup slave address
   I2caRegs.I2CSAR = msg->SlaveAddress;

   // Check if bus busy
   if (I2caRegs.I2CSTR.bit.BB == 1)
   {
      return I2C_BUS_BUSY_ERROR;
   }

   // Setup number of bytes to send
   // MsgBuffer + Address
   I2caRegs.I2CCNT = msg->NumOfBytes+2;

   // Setup data to send
   I2caRegs.I2CDXR = msg->MemoryHighAddr;
   I2caRegs.I2CDXR = msg->MemoryLowAddr;
// for (i=0; i<msg->NumOfBytes-2; i++)
   for (i=0; i<msg->NumOfBytes; i++)

   {
      I2caRegs.I2CDXR = *(msg->MsgBuffer+i);
   }

   // Send start as master transmitter
   I2caRegs.I2CMDR.all = 0x6E20;

   return I2C_SUCCESS;
}

有两个疑问:一是为何要先判断STP位,再判断BB位而不是只判断BB位或是顺序反过来判断?个人理解是BB位既然表示线路是否忙,那即便STP=1时,BB应该总是为1状态吧。二是为何在发送时,先往I2CDXR发送两字节地址,再接着发送四字节数据后才配置I2CMDR且同时置STT,STP和IRS。个人理解是否应先置STT位,在一个一个的发数据,若是没有先置位STT,那先前发送的六个数据(两个地址,四个数据)怎么发送FIFO也就4个容量。而且STT和STP以及IRS是同时置位的,这就不明白了,手册上讲复位时写STT,STP是无效的,那这样配置是否有效,同时置STT和STP又是什么意思。