This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335PGFA 启动瞬间IO引脚电平?



你好,我想问一下, TMS320F28335PGFA  176Pin ,上电瞬间,DSP还没有初始化完成,此时I/O引脚输出是高电平、低电平还是高阻态?

  • “我想问一下, TMS320F28335PGFA 176Pin ,上电瞬间,DSP还没有初始化完成,此时I/O引脚输出是高电平、低电平还是高阻态?”
    Eric:
    见手册如下说明。0~11高组态,12~87高电平。
    All GPIO pins are I/O/Z and have an internal pullup, which can be selectively
    enabled or disabled on a per-pin basis. This feature only applies to the GPIO pins. The pullups on
    GPIO0–GPIO11 pins are not enabled at reset. The pullups on GPIO12–GPIO87 are enabled upon reset.