This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C28346 CAN self-test自环测试

Other Parts Discussed in Thread: TMS320C28346, CONTROLSUITE

Dear TI engineer,

请问对于TMS320C28346 DSP,如何实现一个CAN控制器的自环测试? 硬件上是通过CAN收发器直接将发送光口和接收光口通过光纤互连吗?

谢谢

  • 你需要参考下手册,CAN内部可以配置成内部互联。
  • 您可以看一下

    http://www.ti.com/lit/ug/sprueu0/sprueu0.pdf

    的 Table 2-11. Master Control Register (CANMC) Field Descriptions

    C:\ti\controlSUITE\device_support\c2834x\v112\DSP2834x_examples_ccsv4\ecan_back2back 内是有对应例程的

    // TI File $Revision: /main/3 $
    // Checkin $Date: June 28, 2010   09:18:07 $
    //###########################################################################
    //
    // FILE:    Example_2834xECanBack2Back.c
    //
    // TITLE:   DSP2834x eCAN Back-to-back transmission and reception in
    //          SELF-TEST mode
    //
    // ASSUMPTIONS:
    //
    //    This program requires the DSP2834x header files.
    //
    //    This progrm uses the peripheral's self test mode.
    //    Other then boot mode configuration, no other hardware configuration
    //    is required.
    //
    //    As supplied, this project is configured for "boot to SARAM"
    //    operation.  The 2834x Boot Mode table is shown below.
    //    For information on configuring the boot mode of an eZdsp,
    //    please refer to the documentation included with the eZdsp,
    //
    //       $Boot_Table:
    //
    //         GPIO87   GPIO86     GPIO85   GPIO84
    //          XA15     XA14       XA13     XA12
    //           PU       PU         PU       PU
    //        ==========================================
    //            1        1          1        1    TI Test Only
    //            1        1          1        0    SCI-A boot
    //            1        1          0        1    SPI-A boot
    //            1        1          0        0    I2C-A boot timing 1
    //            1        0          1        1    eCAN-A boot timing 1
    //            1        0          1        0    McBSP-A boot
    //            1        0          0        1    Jump to XINTF x16
    //            1        0          0        0    Jump to XINTF x32
    //            0        1          1        1    eCAN-A boot timing 2
    //            0        1          1        0    Parallel GPIO I/O boot
    //            0        1          0        1    Parallel XINTF boot
    //            0        1          0        0    Jump to SARAM	    <- "boot to SARAM"
    //            0        0          1        1    Branch to check boot mode
    //            0        0          1        0    I2C-A boot timing 2
    //            0        0          0        1    Reserved
    //            0        0          0        0    TI Test Only
    //                                              Boot_Table_End$$
    //
    // DESCRIPTION:
    //
    //    This test transmits data back-to-back at high speed without
    //    stopping.
    //    The received data is verified. Any error is flagged.
    //    MBX0 transmits to MBX16, MBX1 transmits to MBX17 and so on....
    //    This program illustrates the use of self-test mode
    //
    //###########################################################################
    // Original Author H.J.
    //
    // $TI Release: 2834x Header Files V1.12 $
    // $Release Date: March 2011 $
    //###########################################################################
    
    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    
    // Prototype statements for functions found within this file.
    void mailbox_check(int32 T1, int32 T2, int32 T3);
    void mailbox_read(int16 i);
    
    // Global variable for this example
    Uint32  ErrorCount;
    Uint32  PassCount;
    Uint32  MessageReceivedCount;
    
    Uint32  TestMbox1 = 0;
    Uint32  TestMbox2 = 0;
    Uint32  TestMbox3 = 0;
    
    void main(void)
    {
    
        Uint16  j;
    
    // eCAN control registers require read/write access using 32-bits.  Thus we
    // will create a set of shadow registers for this example.  These shadow
    // registers will be used to make sure the access is 32-bits and not 16.
       struct ECAN_REGS ECanaShadow;
    
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP2834x_SysCtrl.c file.
       InitSysCtrl();
    
    // Step 2. Initalize GPIO:
    // This example function is found in the DSP2834x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio();  // Skipped for this example
    
    // For this example, configure CAN pins using GPIO regs here
    // This function is found in DSP2834x_ECan.c
       InitECanGpio();
    
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
       DINT;
    
    // Initialize PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the DSP2834x_PieCtrl.c file.
       InitPieCtrl();
    
    // Disable CPU interrupts and clear all CPU interrupt flags:
       IER = 0x0000;
       IFR = 0x0000;
    
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in DSP2834x_DefaultIsr.c.
    // This function is found in DSP2834x_PieVect.c.
       InitPieVectTable();
    
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in DSP2834x_InitPeripherals.c
    // InitPeripherals(); // Not required for this example
    
    // Step 5. User specific code, enable interrupts:
    
        MessageReceivedCount = 0;
        ErrorCount = 0;
        PassCount = 0;
    
    	InitECana(); // Initialize eCAN-A module
    
        // Mailboxs can be written to 16-bits or 32-bits at a time
        // Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15
        ECanaMboxes.MBOX0.MSGID.all = 0x9555AAA0;
        ECanaMboxes.MBOX1.MSGID.all = 0x9555AAA1;
        ECanaMboxes.MBOX2.MSGID.all = 0x9555AAA2;
        ECanaMboxes.MBOX3.MSGID.all = 0x9555AAA3;
        ECanaMboxes.MBOX4.MSGID.all = 0x9555AAA4;
        ECanaMboxes.MBOX5.MSGID.all = 0x9555AAA5;
        ECanaMboxes.MBOX6.MSGID.all = 0x9555AAA6;
        ECanaMboxes.MBOX7.MSGID.all = 0x9555AAA7;
        ECanaMboxes.MBOX8.MSGID.all = 0x9555AAA8;
        ECanaMboxes.MBOX9.MSGID.all = 0x9555AAA9;
        ECanaMboxes.MBOX10.MSGID.all = 0x9555AAAA;
        ECanaMboxes.MBOX11.MSGID.all = 0x9555AAAB;
        ECanaMboxes.MBOX12.MSGID.all = 0x9555AAAC;
        ECanaMboxes.MBOX13.MSGID.all = 0x9555AAAD;
        ECanaMboxes.MBOX14.MSGID.all = 0x9555AAAE;
        ECanaMboxes.MBOX15.MSGID.all = 0x9555AAAF;
    
        // Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
        ECanaMboxes.MBOX16.MSGID.all = 0x9555AAA0;
        ECanaMboxes.MBOX17.MSGID.all = 0x9555AAA1;
        ECanaMboxes.MBOX18.MSGID.all = 0x9555AAA2;
        ECanaMboxes.MBOX19.MSGID.all = 0x9555AAA3;
        ECanaMboxes.MBOX20.MSGID.all = 0x9555AAA4;
        ECanaMboxes.MBOX21.MSGID.all = 0x9555AAA5;
        ECanaMboxes.MBOX22.MSGID.all = 0x9555AAA6;
        ECanaMboxes.MBOX23.MSGID.all = 0x9555AAA7;
        ECanaMboxes.MBOX24.MSGID.all = 0x9555AAA8;
        ECanaMboxes.MBOX25.MSGID.all = 0x9555AAA9;
        ECanaMboxes.MBOX26.MSGID.all = 0x9555AAAA;
        ECanaMboxes.MBOX27.MSGID.all = 0x9555AAAB;
        ECanaMboxes.MBOX28.MSGID.all = 0x9555AAAC;
        ECanaMboxes.MBOX29.MSGID.all = 0x9555AAAD;
        ECanaMboxes.MBOX30.MSGID.all = 0x9555AAAE;
        ECanaMboxes.MBOX31.MSGID.all = 0x9555AAAF;
    
        // Configure Mailboxes 0-15 as Tx, 16-31 as Rx
        // Since this write is to the entire register (instead of a bit
        // field) a shadow register is not required.
        ECanaRegs.CANMD.all = 0xFFFF0000;
    
        // Enable all Mailboxes */
        // Since this write is to the entire register (instead of a bit
        // field) a shadow register is not required.
        ECanaRegs.CANME.all = 0xFFFFFFFF;
    
        // Specify that 8 bits will be sent/received
        ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
        ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
    
    
        // Write to the mailbox RAM field of MBOX0 - 15
        ECanaMboxes.MBOX0.MDL.all = 0x9555AAA0;
        ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX1.MDL.all = 0x9555AAA1;
        ECanaMboxes.MBOX1.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX2.MDL.all = 0x9555AAA2;
        ECanaMboxes.MBOX2.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX3.MDL.all = 0x9555AAA3;
        ECanaMboxes.MBOX3.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX4.MDL.all = 0x9555AAA4;
        ECanaMboxes.MBOX4.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX5.MDL.all = 0x9555AAA5;
        ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX6.MDL.all = 0x9555AAA6;
        ECanaMboxes.MBOX6.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX7.MDL.all = 0x9555AAA7;
        ECanaMboxes.MBOX7.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX8.MDL.all = 0x9555AAA8;
        ECanaMboxes.MBOX8.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX9.MDL.all = 0x9555AAA9;
        ECanaMboxes.MBOX9.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX10.MDL.all = 0x9555AAAA;
        ECanaMboxes.MBOX10.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX11.MDL.all = 0x9555AAAB;
        ECanaMboxes.MBOX11.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX12.MDL.all = 0x9555AAAC;
        ECanaMboxes.MBOX12.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX13.MDL.all = 0x9555AAAD;
        ECanaMboxes.MBOX13.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX14.MDL.all = 0x9555AAAE;
        ECanaMboxes.MBOX14.MDH.all = 0x89ABCDEF;
    
        ECanaMboxes.MBOX15.MDL.all = 0x9555AAAF;
        ECanaMboxes.MBOX15.MDH.all = 0x89ABCDEF;
    
        // Since this write is to the entire register (instead of a bit
        // field) a shadow register is not required.
        EALLOW;
        ECanaRegs.CANMIM.all = 0xFFFFFFFF;
    
        // Configure the eCAN for self test mode
        // Enable the enhanced features of the eCAN.
        EALLOW;
        ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
        ECanaShadow.CANMC.bit.STM = 1;    // Configure CAN for self-test mode
        ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
        EDIS;
    
        // Begin transmitting
        for(;;)
        {
    
           ECanaRegs.CANTRS.all = 0x0000FFFF;  // Set TRS for all transmit mailboxes
           while(ECanaRegs.CANTA.all != 0x0000FFFF ) {}  // Wait for all TAn bits to be set..
           ECanaRegs.CANTA.all = 0x0000FFFF;   // Clear all TAn
           MessageReceivedCount++;
    
           //Read from Receive mailboxes and begin checking for data */
           for(j=0; j<16; j++)         // Read & check 16 mailboxes
           {
              mailbox_read(j);         // This func reads the indicated mailbox data
              mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
           }
        }
    }
    
    // This function reads out the contents of the indicated
    // by the Mailbox number (MBXnbr).
    void mailbox_read(int16 MBXnbr)
    {
       volatile struct MBOX *Mailbox;
       Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
       TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
       TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
       TestMbox3 = Mailbox->MSGID.all;// = 0x9555AAAn (n is the MBX number)
    
    } // MSGID of a rcv MBX is transmitted as the MDL data.
    
    
    void mailbox_check(int32 T1, int32 T2, int32 T3)
    {
        if((T1 != T3) || ( T2 != 0x89ABCDEF))
        {
           ErrorCount++;
        }
        else
        {
           PassCount++;
        }
    }
    
    
    //===========================================================================
    // No more.
    //===========================================================================
    

  • 谢谢,我看看。
  • 谢谢,我先学习一下。
  • 我先学习,谢谢。