This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想用一个gpio作为TZ1信号去封pwm,这块跟335不太一样,主要设计xbar的设置,请TI或其他技术大牛,提供一下支持,这块应该怎么设置。多谢!
//########################################################################### // // FILE: epwm_trip_zone.c // // TITLE: ePWM module using Trip-Zone submodule. // //! \addtogroup cpu01_example_list //! <h1> EPWM Trip Zone Module (epwm_trip_zone)</h1> //! //! This example configures ePWM1 and ePWM2 as follows //! - ePWM1 has TZ1 as one shot trip source //! - ePWM2 has TZ1 as cycle by cycle trip source //! //! Initially tie TZ1 high. During the test, monitor ePWM1 or ePWM2 //! outputs on a scope. Pull TZ1 low to see the effect. //! //! \b External \b Connections \n //! - EPWM1A is on GPIO0 //! - EPWM2A is on GPIO2 //! - TZ1 is on GPIO12 //! //! This example also makes use of the Input X-BAR. GPIO12 (the external //! trigger) is routed to the input X_BAR, from which it is routed to TZ1. //! //! The TZ-Event is defined such that EPWM1A will undergo a One-Shot Trip //! and EPWM2A will undergo a Cycle-By-Cycle Trip. //! // _____________ __________________ // | | | | // GPIO12 -----| I/P X-BAR |-----TZ1-----| ePWM TZ Module |-----TZ-Event // |___________| |________________| // // // //########################################################################### // $TI Release: F2837xS Support Library v210 $ // $Release Date: Tue Nov 1 15:35:23 CDT 2016 $ // $Copyright: Copyright (C) 2014-2016 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### // // Included Files // #include "F28x_Project.h" // // Defines // #define EXTTrig // Leave Uncommented for Testing with External Trigger. // Comment for Testing with ePWM Trigger. // // Globals // Uint32 EPwm1TZIntCount; Uint32 EPwm2TZIntCount; // // Function Prototypes // void InitEPwm1Example(void); void InitEPwm2Example(void); void InitTzGpio(void); __interrupt void epwm1_tzint_isr(void); __interrupt void epwm2_tzint_isr(void); void InitEPwmGpio_TZ(void); // // Main // void main(void) { // // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xS_SysCtrl.c file. // InitSysCtrl(); // // Step 2. Initialize GPIO: // This example function is found in the F2837xS_Gpio.c file and // illustrates how to set the GPIO to it's default state. // // InitGpio(); // // enable PWM1, and PWM2 // CpuSysRegs.PCLKCR2.bit.EPWM1=1; CpuSysRegs.PCLKCR2.bit.EPWM2=1; // // For this case just init GPIO pins for ePWM1, ePWM2, ePWM3 // InitEPwmGpio_TZ(); InitTzGpio(); // // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // DINT; // // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2837xS_PieCtrl.c file. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags: // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in F2837xS_DefaultIsr.c. // This function is found in F2837xS_PieVect.c. // InitPieVectTable(); // // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. // EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.EPWM1_TZ_INT = &epwm1_tzint_isr; PieVectTable.EPWM2_TZ_INT = &epwm2_tzint_isr; EDIS; // This is needed to disable write to EALLOW protected registers // // Step 4. Initialize the Device Peripherals: // EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0; EDIS; InitEPwm1Example(); InitEPwm2Example(); EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1; EDIS; // // Step 5. User specific code, enable interrupts: // EPwm1TZIntCount = 0; EPwm2TZIntCount = 0; // // Enable CPU INT2 which is connected to EPWM1-3 INT: // IER |= M_INT2; // // Enable EPWM INTn in the PIE: Group 3 interrupt 1-3 // PieCtrlRegs.PIEIER2.bit.INTx1 = 1; PieCtrlRegs.PIEIER2.bit.INTx2 = 1; // // Enable global Interrupts and higher priority real-time debug events: // EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // // Step 6. IDLE loop. Just sit and loop forever (optional): // for(;;) { asm (" NOP"); } } // // epwm1_tzint_isr - EPWM1 TZ ISR // __interrupt void epwm1_tzint_isr(void) { EPwm1TZIntCount++; // // To Re-enable the OST Interrupt, do the following: // EALLOW; // EPwm1Regs.TZCLR.bit.OST = 1; // EPwm1Regs.TZCLR.bit.INT = 1; // EDIS; // // // Acknowledge this interrupt to receive more interrupts from group 2 // PieCtrlRegs.PIEACK.all = PIEACK_GROUP2; } // // epwm2_tzint_isr - EPWM2 TZ ISR // __interrupt void epwm2_tzint_isr(void) { GpioDataRegs.GPATOGGLE.bit.GPIO11 = 1; EPwm2TZIntCount++; // // Clear the flags - we will continue to take // this interrupt until the TZ pin goes high // EALLOW; EPwm2Regs.TZCLR.bit.CBC = 1; EPwm2Regs.TZCLR.bit.INT = 1; EDIS; // // Acknowledge this interrupt to receive more interrupts from group 2 // PieCtrlRegs.PIEACK.all = PIEACK_GROUP2; } // // InitEPwm1Example - Initialize EPWM1 configuration // void InitEPwm1Example() { // // Enable TZ1 as one shot trip sources // EALLOW; EPwm1Regs.TZSEL.bit.OSHT1 = 1; // // Set TZA // EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_HI; // // Enable TZ interrupt // EPwm1Regs.TZEINT.bit.OST = 1; EDIS; EPwm1Regs.TBPRD = 12000; // Set timer period EPwm1Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0 EPwm1Regs.TBCTR = 0x0000; // Clear counter // // Setup TBCLK // EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4; // Clock ratio to SYSCLKOUT EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV4; EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // // Setup compare // EPwm1Regs.CMPA.bit.CMPA = 6000; // // Set actions // EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on CAU EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM1A on CAD } // // InitEPwm2Example - Initialize EPWM2 configuration // void InitEPwm2Example() { // // Enable TZ1 as one cycle-by-cycle trip sources // EALLOW; EPwm2Regs.TZSEL.bit.CBC1 = 1; // // Set TZA // EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_HI; // // Enable TZ interrupt // EPwm2Regs.TZEINT.bit.CBC = 1; EDIS; EPwm2Regs.TBPRD = 6000; // Set timer period EPwm2Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0 EPwm2Regs.TBCTR = 0x0000; // Clear counter // // Setup TBCLK // EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4; // Clock ratio to SYSCLKOUT EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV4; // Slow just to observe on // the scope. // // Setup compare // EPwm2Regs.CMPA.bit.CMPA = 3000; // // Set actions // EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM2A on CAU EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM2A on CAD } // // InitTzGpio - Initialize TZ GPIOs // void InitTzGpio(void) { // // For External Trigger, GPIO12 as the trigger for TripZone // GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up on GPIO12 (TZ1) GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3; // Asynch input GPIO12 (TZ1) EALLOW; InputXbarRegs.INPUT1SELECT = 12; EDIS; // // For monitoring when the TZ Interrupt has been entered // EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO11 = 1; // Disable pull-up on GPIO0 (EPWM1A) GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0; // Configure GPIO0 as EPWM1A GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; EDIS; } // // InitEPwmGpio_TZ - Initialize EPWM1A and EPWM2A GPIOs // void InitEPwmGpio_TZ(void) { EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; // Disable pull-up on GPIO0 (EPWM1A) GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A GpioCtrlRegs.GPAPUD.bit.GPIO2 = 1; // Disable pull-up on GPIO2 (EPWM2A) GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // Configure GPIO2 as EPWM2A EDIS; } // // End of file //