This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335串口烧写程序(CKFA)



专家好: 

    参考TMS320F281x Boot ROM Serial Flash Programming,本人需要用MFC编写一个28335串口烧写软件,有一些疑问:发送"a"锁定波特率后,然后放送CKFA.bin(Flash Api),Api为TI官网例程,没有修改,发送的过程成功,每发送一个8位数据DSP响应发回一位,发送完毕后,但是DSP没有自动运行CKFA!

    问题:

    1.通过串口发送CKFA.bin(附件),DSP保存CKFA的位置?

    1.DSP保存CKFA的位置是M0、M1 SARAM?Unsecured Ram是哪个空间?Unsecured Ram空间大小是否满足CKFA要求?

    2.CKFA的Entry Point应该是多少?我编译TI官网例程CKFA的Entry Point为0x00338166,发送CKFA后没有自动运行时由于Entry Point的原因吗?

    3.需要修改CMD文件(附件)吗?

希望各位大虾指点一下,万分感激啊!

Bin文件andCMD文件.zip