This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S 有几个SDAA、SCLA脚,请问要怎么选择?



  • 您可以看一下数据手册 www.ti.com.cn/.../tms320f28377s.pdf 的Table 4-3

    Table 4-3 shows the GPIO muxed pins. The default for each pin is the GPIO function, secondary functions can be selected by setting both the GPyGMUXn.GPIOz and GPyMUXn.GPIOz register bits. The GPyGMUXn register should be configured prior to the GPyMUXn to avoid transient pulses on GPIO's from alternate mux selections.

    您可以通过上面提到的寄存器来进行选择