This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36下载C28程序下不进去

Other Parts Discussed in Thread: CONTROLSUITE

下载的时候提示

Cortex_M3_0: GEL Output: Memory Map Initialization Complete
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: GEL Output:
RAM Initialization Complete
C28xx_0: Flash Programmer: Unable to acquire the pump semaphore. The other core might still be accessing the pump registers. Operation Cancelled.
C28xx_0: File Loader: Memory write failed: Unknown error
C28xx_0: GEL: File: D:\wwj\F28M36-F28\Flash\F28M36-F28.out: Load failed.

请教这个问题是怎么回事?我的环境是CCS8.2

  • 请问您是下载的 C:\ti\controlSUITE\device_support\f28m36x\v220\F28M36x_examples_Control 内的例程?

    建议您先看一下doc文件内的文档 F28M36x-FRM-EX-UG.pdf

    Note: In order to run and debug Control subsystem examples, the M3 core must run first and initialize the Control subsystem and GPIOs. Within the F28M36x_examples_Control directory, the example, setup_m3, is provided for this purpose.
  • 不是的,这个是我们旧产品的控制程序,我先下载了M3的代码,但是,下载C28代码的时候就提示这个错误,不知道以前是怎么操作的。

    您说的这个文件我先看下,但是我这里只有到209,不知道是否一致?

  • 还有,这个文档近200页,要一字一句的看完?
  • 亲,稍安毋躁

    您现在是烧录的双核Dual的程序?

    您只需要看文档内的第二章 Getting Started and Troubleshooting 关于如何配置及调试烧录程序即可,文档内剩余部分是关于例程介绍的,您无需关注。

    第二章 Getting Started and Troubleshooting 一步步地介绍了相关的步骤,您可以根据提示先尝试操作一下,是否是您的配置或其他步骤有问题。

    或者您也可以先尝试烧录下TI的例程试试

    祝你成功