This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题描述:DP83822的硬件电路设计原理图已验证是可用的,而且芯片的配置电路是默认将DP83822配置为MII接口;在重新做板后发现该模块不能正常获取IP,测量信号发现TX_CLK和RX_CLK没有时钟输出,RX_D3/GPIO3却有50MHz的时钟输出,MDC和MDIO可正常读取和配置寄存器,个人认为芯片工作正常,但是硬件默认的配置接口却变成了RMII接口,硬件电路设计并未更改,之前可正常配置为MII;
由于硬件电路不知如何修改,也不太方便修改,能否在芯片复位后通过软件配置寄存器的方法,将RMII接口配置为MII接口,本人尝试过配置0x0017的bit9和bit5,但似乎不止修改这些,请问该如何配置寄存器才能更改为MII接口;
还望各位大佬多多指点,非常感谢!