This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377的DMA使用问题

大家好:我通过DMA实现对外设进行控制。具体情况是这样的:外设是外部Flash接口符合SPI协议,我仿照例程进行改写,实现可以通过DMA实现对外设Flash进行读写。首先,我根据Flash的命令格式,实现通过CPU控制SPI实现对Flash进行读写,这步调试完毕。之后想通过DMA对Flash进行操作。

问题1:在程序中,如果一开始不用DMA,只通过SPI可以对Flash进行操作。只要一使用DMA,在切换到SPI操作Flash读取数据就不正常了。这是为什么?

问题2:通过DMA对外设Flash读取数据时,好像多了一个无效数据,导致最后一个数据丢失,这是为什么?

问题3:DMA中断应该是将所有数据传完才进中断的吧?为什么我观察到的现象是进入中断时,还有几个数据还在传输?

期望大神的指点,谢谢!