原理图这样设置的:
1、Vdd、VDDIO、VddA、Vdd3VFL全部都连接到同一个3.3V电源,Vss、VssA都连到GND;
2、VREGENZ接地;
3、XRS串联2K电阻到3.3V;
现在存在问题是,上电后,XRS引脚一直为低;
难道是Vdd、VDDIO、VddA同时上电引起内部电源监测出错引起复位的,需要对Vdd、VDDIO的时序进行处理?还是其他引脚设置不对引起的?
请有使用过此芯片的大虾解答一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Vdd不能接3.3V。如果你把VREGENZ接地,使用内部LDO的话,Vdd只接电容。