This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F021_API_F2837xD_FPU32.lib的作用?

Other Parts Discussed in Thread: CONTROLSUITE

F021_API_F2837xD_FPU32.lib的作用?和rts2800_fpu32有什么区别与联系吗

  • 我们是有专门的文档介绍的

    The Flash API is a library of routines, that when called with the proper parameters in the proper sequence, erases, programs, or verifies Flash memory. Flash API can be used to program and verify the OTP memory as well.

    路径如下 C:\ti\controlSUITE\device_support\F2837xD\v210\doc\FlashAPI_Doc

    如果安装了TI ControlSUITE,则可以获取示例代码 。

    (如果使用了默认安装目录):

    C:\ ti \ controlSUITE \ device_support \ F2837xD \ v210 \ F2837xD_examples_Dual \ flash_programming