This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用官方例程,软件触发采集,用50K的滑动变阻器接到评估板上的3.3V和GND,测量中间管脚的电压,发现有一个问题:
1.如果按照官方给的ADC Acquisition时间为75ns,采集的值和万用表采集的不一样(两者一起接到管脚上),而且改变ADC Acquisition的时间可以改变ADC采集的值,最后发现大约在2us左右和万用表测的值差不多,按这么说的话是不是说内部12位ADC采集速率达不到3.5M?
2.我个人觉得是因为管脚50K下拉电阻的影响,如果是这样的话,是不是说ADC测量只能测电阻远小于50K时候的电压,否则必须增大ADC Acquisition的时间?