This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

280049加密后无法独立上电运行问题



使用280049加密后(加密只用了Z1区),连接仿真器,在On-chip Flash中解密,load程序,可以运行,

但是断开仿真器后重新上电无法正常运行,DSP一直处于复位状态

分析原因:1、解密问题

2、boot 模式问题

针对1解密,直接调用的TI  driver lab中的解密函数DCSM_unlockZone1CSM(&PasswordKey),问题依旧

对于2 Boot,采用硬件默认boot模式,也就是gpio32、gpio24上拉高电平,因此将Z1otp-GPREG1配置成0xFFFFFFFF,Z1otp-bootctrl为0xFFFFFFFF出现问题后,将1otp-GPREG1(0x7800C)配置成0x5AFFFFFF,Z1otp-bootctrl(0x7801E)为0xFFFFFF02,问题依旧

请问各位大神还有其他可能的原因么,多谢!