Other Parts Discussed in Thread: TMS320F28377S
TMS320F28377s的数据表中
ERRORSTS引脚的描述为:Error status output. This pin has an internal pulldown。
它的功能是检测28377s芯片的工作状态是否出现问题吗?
可以不使用这个引脚的功能吗,如果不使用怎么处理这个引脚,接上拉电阻还是电容接地?
(谢谢你抽空回答这个问题~)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F28377S
TMS320F28377s的数据表中
ERRORSTS引脚的描述为:Error status output. This pin has an internal pulldown。
它的功能是检测28377s芯片的工作状态是否出现问题吗?
可以不使用这个引脚的功能吗,如果不使用怎么处理这个引脚,接上拉电阻还是电容接地?
(谢谢你抽空回答这个问题~)
谢谢mangui zhang的回答!
您可以看一下www.ti.com/.../spruhx5e.pdf 的2.6.8 ERRORSTS Pin给出的具体描述
The ERRORSTS pin is an ‘always output’ pin and remains low until an error is detected inside the chip. On an error, the ERRORSTS pin goes high until the corresponding internal error status flag for that error source is cleared.
The ERRORSTS pin will be tri-stated until the chip power rails ramp up to the lower operational limit. As the ERRORSTS pin is an active-high pin, users who care about the state of this pin during power-up should connect an external pull-down on this pin.
ERRORSTS引脚一直保持low直到有error发生(变为高电平),该引脚主要是用于指示是否有对应的error发生
关于不使用这个引脚的功能,数据手册给出了相关的说明

4.5 Connections for Unused Pins
ERRORSTS No Connect