各位午安,我最近在用F28335对ADC采样得到的数据作FFT,遇到了一个问题:由于F28335的ADC采样率的限制,我的采样点数无法做到恰好是2的整数次幂(目前采样点数设为500);而我所用的FFT模板的输入点数是2的整数次幂(原始点数128);我可以直接用500点的采样数据作为输入吗?会不会出现问题?恳请各位不吝赐教,下附我用的FFT模板代码:
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include"math.h" #define PI 3.1415926 #define SAMPLENUMBER 128 void InitForFFT(); void MakeWave(); //void FFT(float dataR[SAMPLENUMBER],float dataI[SAMPLENUMBER]); int INPUT[SAMPLENUMBER],DATA[SAMPLENUMBER]; float fWaveR[SAMPLENUMBER],fWaveI[SAMPLENUMBER],w[SAMPLENUMBER]; float sin_tab[SAMPLENUMBER],cos_tab[SAMPLENUMBER]; void FFT(float dataR[SAMPLENUMBER],float dataI[SAMPLENUMBER]) { int x0,x1,x2,x3,x4,x5,x6,xx; int i,j,k,b,p,L; float TR,TI,temp; /********** following code invert sequence ************/ for ( i=0;i<SAMPLENUMBER;i++ ) { x0=x1=x2=x3=x4=x5=x6=0; x0=i&0x01; x1=(i/2)&0x01; x2=(i/4)&0x01; x3=(i/8)&0x01;x4=(i/16)&0x01; x5=(i/32)&0x01; x6=(i/64)&0x01; xx=x0*64+x1*32+x2*16+x3*8+x4*4+x5*2+x6; dataI[xx]=dataR[i]; } for ( i=0;i<SAMPLENUMBER;i++ ) { dataR[i]=dataI[i]; dataI[i]=0; } /************** following code FFT *******************/ for ( L=1;L<=7;L++ ) { /* for(1) */ b=1; i=L-1; while ( i>0 ) { b=b*2; i--; } /* b= 2^(L-1) */ for ( j=0;j<=b-1;j++ ) /* for (2) */ { p=1; i=7-L; while ( i>0 ) /* p=pow(2,7-L)*j; */ { p=p*2; i--; } p=p*j; for ( k=j;k<128;k=k+2*b ) /* for (3) */ { TR=dataR[k]; TI=dataI[k]; temp=dataR[k+b]; dataR[k]=dataR[k]+dataR[k+b]*cos_tab[p]+dataI[k+b]*sin_tab[p]; dataI[k]=dataI[k]-dataR[k+b]*sin_tab[p]+dataI[k+b]*cos_tab[p]; dataR[k+b]=TR-dataR[k+b]*cos_tab[p]-dataI[k+b]*sin_tab[p]; dataI[k+b]=TI+temp*sin_tab[p]-dataI[k+b]*cos_tab[p]; } /* END for (3) */ } /* END for (2) */ } /* END for (1) */ for ( i=0;i<SAMPLENUMBER/2;i++ ) { w[i]=sqrt(dataR[i]*dataR[i]+dataI[i]*dataI[i]); } } /* END FFT */ void InitForFFT() { int i; for ( i=0;i<SAMPLENUMBER;i++ ) { sin_tab[i]=sin(PI*2*i/SAMPLENUMBER); cos_tab[i]=cos(PI*2*i/SAMPLENUMBER); } } void MakeWave() { int i; for ( i=0;i<SAMPLENUMBER;i++ ) { INPUT[i]=sin(PI*2*i/SAMPLENUMBER*3)*1024; } } void main(void) { int i; // Step 1. Initialize System Control: InitSysCtrl(); // Step 2. Initalize GPIO: // InitGpio(); Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; InitPieCtrl(); IER = 0x0000; IFR = 0x0000; InitPieVectTable(); // Step 4. InitForFFT(); MakeWave(); for ( i=0;i<SAMPLENUMBER;i++ ) { fWaveR[i]=INPUT[i]; fWaveI[i]=0.0f; w[i]=0.0f; } FFT(fWaveR,fWaveI); for ( i=0;i<SAMPLENUMBER;i++ ) { DATA[i]=w[i]; } for(;;) { } //break point }