This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335上电顺序需要写软件进行规定吗?例如内核1.9V电压和IO口3.3V电压,能否写程序改变上电顺序?



28335的内核1.9V电压和IO口3.3V电压的上电顺序可以用软件来规定吗?还是它自己在BootLoader里面已经规定好了的,如果我想更改上电顺序,我应该在哪里设置或者更改。

  • 请您参考一下

    www.ti.com.cn/.../tms320f28335.pdf

    芯片工作没有上电顺序要求。但还是建议注意下面的话

    "However, if the 3.3-V transistors in the level shifting output buffers of the I/O pins are powered prior to the 1.9-V transistors, it is possible for the output buffers to turn on, causing a glitch to occur on the pin during power up. To avoid this behavior, power the VDD pins prior to or simultaneously with the VDDIO pins, ensuring that the VDD pins have reached 0.7 V before the VDDIO pins reach 0.7 V."

    如果VDD比VDDIO慢到达0.7V的话,上电时有可能出现一个小脉冲。

  • MCU的上电顺序都是外部硬件设计决定的 不会在bootloader级进行控制
    控制上电顺序的最主要原因是合理的上电顺序让MCU启动加载运行正常
    其次就是避免上电瞬间过高的电流冲击