This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28035系列UL1998标准认证事宜(Using 28035 serial chip for UL1998 Standard)



目前我正在使用TI的28035系列芯片进行UL1998的认证工作,其中包含有一些微电子故障检测,具体如下:

1、CPU故障检测(主要是PC/SP/以及一些特殊寄存器(如状态寄存器)是否能够正常使用)

2、RAM检测,通过对RAM的全部地址的读写,确保RAM无读写问题

3、FLASH检测,主要是确认FLASH中存放的运行代码块不会发生篡改

等上述主要描述

是否能提供一些相关技术文档帮助整理检测代码开发思路

I am a developer of MCU, recent days ,I am using 28035 serial MCU for UL1998 Standard certification.The following are some microelectronic fault check:

1.CPU Check, To confirm PC/SP and other special register works normally

2、RAM check, to complete read and write all address of ram to make sure ram works fine

3、FLASH check, to confirm there is no unnormal  rectification  in flash range of code

It is very kind of you to provide some suggestions or some technical documents,thans