This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 问题



弱弱的问一下几个问题,谢谢解惑:

1. 我在X1和X2之间接30MHz晶振,XCLKIN接地,XCLKOUT应该怎么接?

2.28335的XRD(外部接口读使能)管脚应该怎么接?

3.ADC模块的3.3V、1.8V模拟电源和模拟地能不能和数字3.3V、1.8V、数字地接在一起?

4.ADCREFIN(外部参考输入)是做什么用的,应该怎么接?

5.没有用到的GPIO管脚和ADCINx应该怎么处理?

  • 1. XCLKOUT可以悬空

    2.连接外部RAM的使能引脚;如果没有用外部RAM可以悬空

    3.可以,但是建议模拟和数字电源间串联电感,地之间单点连接

    4.一般用ADC的3.3V当做12bit采样信号最大值0xFFF,也可以给ADCREFIN一个小于3.3V的电平,用这个电平作为采样信号最大值0xFFF

    5.没有用到的管脚建议下拉电阻接地

  • 谢谢Terry Deng.

    再问下,使用内部参考电压时,ADCREFIN是不是应该接模拟地,选择使用内部参考电压是通过软件来实现的?