This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用器件:TMS320F28377S,封装为100pin
目的:使EPWM7与EPWM10载波移相180度
操作方法:根据数据手册EPWM7与EPWM10不属于同一个同步链,因此在EPWM7过零的时候产生同步信号,同时选择EMPW10的同步输入源为EPWM7,具体代码如下,结果显示EPWM7和EPWM10移相180度,怀疑EPWM7的同步触发信号未送到EPWM10,是否100pin引脚的不能这样操作?
您可以看一下
14.13.7 Practical Applications Using Phase Control Between PWM Modules
Here, TBPRD = 600 for both master and slave. For the slave, TBPHS = 200 (that is, 200/600 X 360° = 120°).
按照给出的说明
TBPHS/TBPRD X 360° = 180°
您可以试一下