This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 的 ADC模块 读取的值和实测的值会有 100MV以内的误差,请教一下怎么优化?



初始化程序

#if (CPU_FRQ_150MHZ)     // Default - 150 MHz SYSCLKOUT
  #define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3)   = 25.0 MHz
#endif
#if (CPU_FRQ_100MHZ)
  #define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2)   = 25.0 MHz
#endif
void Init_ADC(void)
{
 uint16_t tmp = 0;

 EALLOW;
  SysCtrlRegs.HISPCP.all = ADC_MODCLK; // HSPCLK = SYSCLKOUT/ADC_MODCLK
 EDIS;

 AdcRegs.ADCTRL3.all = 0x00E0;   // Power up bandgap/reference/ADC circuits
 tmp = 5000;
 while(tmp--);     // 等待ADC稳定

 //以下开始设置ADC的控制寄存器、转换通道选择寄存器等
 AdcRegs.ADCST.all = 0x30;   //首先清除中断标志位
 AdcRegs.ADCOFFTRIM.all = 0;
 AdcRegs.ADCTRL3.all = 0x0E2;
 //bit7~6:ADCBGRFDN[1:0]:adc 缝隙上电,3上电
 //bit5:ADCPWDN:adc 模块上电,set1 上电
 //bit1~4:ADCCLKPS=1
 // bit0:SMODE_SEL =0  :set 0   顺序采样;   set1 :同步采样
 // 0 = [ADCCLK = HSPCLK/(CPS+1)], 1 = [ADCCLK = HSPCLK/2*(1)(CPS+1)]; HSPCLK 默认情况下 = CPUSYSCLK/2;
 //ADC module clock = HSPCLK/2*ADC_CKPS   = 25.0MHz/(1*2) = 12.5MHz
//设置为顺序采样模式 0 = 连续采样方式 1 = 并发采样方式
 AdcRegs.ADCTRL1.all = 0x0F50;
 /*bit13~12:SUSMOD=0;
 bit11~8:ACQ_PS =F :16 ADC clocks;
 bit7: CPS =0时钟预分频1
 bit6: CONT_RUN=1;//设置为启停模式 0 = 启停模式,1 = 连续转换模式
 bit5:SEQ_OVRD = 0
 bit4:SEQ_CASC =1//级联模式 0 = 双序列发生器方式, 1 = 级联模式
 */
 //AdcRegs.ADCTRL1.bit.CONT_RUN = 1;

 AdcRegs.ADCTRL2.all = 0x0000;
 AdcRegs.ADCMAXCONV.all = 0x0F;   //最大转换16通道

 AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0;  // ADCINA0 & ADCINB0
 AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 1;  // ADCINA1 & ADCINB1
 AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 2;  // ADCINA2 & ADCINB2
 AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 3;  // ADCINA3 & ADCINB3

 AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 4;  // ADCINA4 & ADCINB4
 AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 5;  // ADCINA5 & ADCINB5
 AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 6;  // ADCINA6 & ADCINB6
 AdcRegs.ADCCHSELSEQ2.bit.CONV07 = 7;  // ADCINA7 & ADCINB7

 AdcRegs.ADCCHSELSEQ3.bit.CONV08 = 8;  // ADCINA8 & ADCINB8
 AdcRegs.ADCCHSELSEQ3.bit.CONV09 = 9;  // ADCINA9 & ADCINB9
 AdcRegs.ADCCHSELSEQ3.bit.CONV10 = 10;  // ADCINA10 & ADCINB10
 AdcRegs.ADCCHSELSEQ3.bit.CONV11 = 11;  // ADCINA11 & ADCINB11

 AdcRegs.ADCCHSELSEQ4.bit.CONV12 = 12;  // ADCINA12 & ADCINB12
 AdcRegs.ADCCHSELSEQ4.bit.CONV13 = 13;  // ADCINA13 & ADCINB13
 AdcRegs.ADCCHSELSEQ4.bit.CONV14 = 14;  // ADCINA14 & ADCINB14
 AdcRegs.ADCCHSELSEQ4.bit.CONV15 = 15;  // ADCINA15 & ADCINB15
}

系统时钟用的是150M

读取结果的函数

void Test_Ai_Handle(Ubyte *paramData)
{
     uint16_t i = 0;
  uint16_t value[16];
  uint16_t chan = 0;
  float tmp = 0;
  uint16_t  delay_tmp = 0;

  chan = paramData[0];
  memset((void *)value, 0, sizeof(value));

  /* handle */
  for(i=0; i<10; i++)//3 change 10
  {
   /* start sw conversion */
   AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;   // Reset SEQ1
   AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;   // sofware start ADC

   /* wait conversion done */
   delay_tmp = 1000;
   while(delay_tmp--);
   while(AdcRegs.ADCST.bit.INT_SEQ1 == 0);

   /* value save */
   value[0] += ((AdcRegs.ADCRESULT0) >> 4);
   value[1] += ((AdcRegs.ADCRESULT1) >> 4);
   value[2] += ((AdcRegs.ADCRESULT2) >> 4);
   value[3] += ((AdcRegs.ADCRESULT3) >> 4);
   value[4] += ((AdcRegs.ADCRESULT4) >> 4);
   value[5] += ((AdcRegs.ADCRESULT5) >> 4);
   value[6] += ((AdcRegs.ADCRESULT6) >> 4);
   value[7] += ((AdcRegs.ADCRESULT7) >> 4);
   value[8] += ((AdcRegs.ADCRESULT8) >> 4);
   value[9] += ((AdcRegs.ADCRESULT9) >> 4);
   value[10] += ((AdcRegs.ADCRESULT10) >> 4);
   value[11] += ((AdcRegs.ADCRESULT11) >> 4);
   value[12] += ((AdcRegs.ADCRESULT12) >> 4);
   value[13] += ((AdcRegs.ADCRESULT13) >> 4);
   value[14] += ((AdcRegs.ADCRESULT14) >> 4);
   value[15] += ((AdcRegs.ADCRESULT15) >> 4);
  }

  tmp = (float)(value[chan-1]) / 10;
  tmp = (3000 * tmp / 4095) ;

  if(tmp >= 1499)
   tmp += 1;
  else;
  paramData[3] = Type_Extrh_U8_Of_U16_TE(tmp);
  paramData[4] = Type_Extrl_U8_Of_U16_TE(tmp);

}

把ADC模块的误差缩小到30MV 以内