This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2808锁住了 求TI的解锁文档

Other Parts Discussed in Thread: TMS320F28335

DSP2808锁住了 求TI的解锁文档

  • 你好,你有解锁的密码吗?如果没有密码的话是没办法解锁的
  • 如果有密码的话可以连接JTAG之后在debug模式下,On-chip-flash 中进行操作解锁。
  • 您有具体的解锁步骤吗?》或者文档

  • 一起自己写过一个,你可以参考一下:

    以F28335为例
    1、配置芯片的GPIO 84~87为1100,使芯片进入Branch to check boot mode模式(详情可参考芯片Datasheet第106页,6.1.9 Boot ROM )。如果是TI购买的F28335 controlCARD(以R2.2为例),那么把controlCARD上SW2开关的1~4分别配置为1100。

    2、打开CCS,连接芯片和PC,上电。配置target configuration(View - Target Configuration),配置完成后Test Connection一下,测试成功后进入下一步。(本来以为直接点击debug就可以了,但实验了几次发现一定要做一下这个步骤才行,否则没办法进入debug模式)

    3、点击小虫子图标进入debug模式,进入之后如果显示没有连接JTAG的话先点击Connect Target连接JTAG,然后点击Tools - On Chip Flash,在On Chip Flash中的Code Security Password - Key0~7中输入正确的密码,然后点击Unlock。这样就解锁了,系统会提示:
    C28xx: GEL Output:
    ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: Flash Programmer: Warning: The configured device (TMS320F28335), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
    C28xx: Starting device unlocking...
    C28xx: Device unlocked. To clear the programmed password, please erase Sector A of Flash memory.
    解锁成功后你就可以正常使用芯片进行烧写flash了。

    4、如果你希望彻底解锁芯片(以后启动都不需要输入密码解锁),那么按照上述系统提示的“To clear the programmed password, please erase Sector A of Flash memory.”操作。接着刚才的步骤,跳到On Chip Flash中的Erase Sector Selection,选择Sector A(默认是全选的),然后点击“Erase Flash”。这样就去掉密码了,系统会提示:
    C28xx: Erasing Flash memory...
    C28xx: GEL Output:
    ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: Operation completed successfully.

    或者也可以把Code Security Password - Key0~7全部改为F,默认就是不加密状态。
    以上就完成了芯片的解锁和清除密码操作了。