28335里面,如何开启和关断epwm_isr中断,epwm_isr中断是怎么触发的,具体的寄存器配置方法是怎么样的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
28335里面,如何开启和关断epwm_isr中断,epwm_isr中断是怎么触发的,具体的寄存器配置方法是怎么样的?
建议您看一下例程,如C:\ti\controlSUITE\device_support\f2833x\v142\DSP2833x_examples_ccsv5\epwm_timer_interrupts
代码如下
//########################################################################### // Description: //! \addtogroup f2833x_example_list //! <h1>ePWM Timer Interrupt (epwm_timer_interrupts)</h1> //! //! This example configures the ePWM Timers and increments a counter each //! time an interrupt is taken. \n //! In this example: //! - All ePWM's are initialized. //! - All timers have the same period. //! - The timers are started sync'ed. //! - An interrupt is taken on a zero event for each ePWM timer. //! - ePWM1: takes an interrupt every event. //! - ePWM2: takes an interrupt every 2nd event. //! - ePWM3: takes an interrupt every 3rd event. //! - ePWM4-ePWM6: takes an interrupt every event. //! //! Thus the Interrupt count for ePWM1, ePWM4, ePWM5, and ePWM6 should be //! equal.The interrupt count for ePWM2 should be about half that of ePWM1 //! and the interrupt count for ePWM3 should be about 1/3 that of ePWM1. //! //! \b Watch \b Variables \n //! - EPwm1TimerIntCount //! - EPwm2TimerIntCount //! - EPwm3TimerIntCount //! - EPwm4TimerIntCount //! - EPwm5TimerIntCount //! - EPwm6TimerIntCount // // //########################################################################### // $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $ // $Release Date: November 1, 2016 $ // $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File // Configure which ePWM timer interrupts are enabled at the PIE level: // 1 = enabled, 0 = disabled #define PWM1_INT_ENABLE 1 #define PWM2_INT_ENABLE 1 #define PWM3_INT_ENABLE 1 #define PWM4_INT_ENABLE 1 #define PWM5_INT_ENABLE 1 #define PWM6_INT_ENABLE 1 // Configure the period for each timer #define PWM1_TIMER_TBPRD 0x1FFF #define PWM2_TIMER_TBPRD 0x1FFF #define PWM3_TIMER_TBPRD 0x1FFF #define PWM4_TIMER_TBPRD 0x1FFF #define PWM5_TIMER_TBPRD 0x1FFF #define PWM6_TIMER_TBPRD 0x1FFF // Prototype statements for functions found within this file. __interrupt void epwm1_timer_isr(void); __interrupt void epwm2_timer_isr(void); __interrupt void epwm3_timer_isr(void); __interrupt void epwm4_timer_isr(void); __interrupt void epwm5_timer_isr(void); __interrupt void epwm6_timer_isr(void); void InitEPwmTimer(void); // Global variables used in this example Uint32 EPwm1TimerIntCount; Uint32 EPwm2TimerIntCount; Uint32 EPwm3TimerIntCount; Uint32 EPwm4TimerIntCount; Uint32 EPwm5TimerIntCount; Uint32 EPwm6TimerIntCount; void main(void) { int i; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.EPWM1_INT = &epwm1_timer_isr; PieVectTable.EPWM2_INT = &epwm2_timer_isr; PieVectTable.EPWM3_INT = &epwm3_timer_isr; PieVectTable.EPWM4_INT = &epwm4_timer_isr; PieVectTable.EPWM5_INT = &epwm5_timer_isr; PieVectTable.EPWM6_INT = &epwm6_timer_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example InitEPwmTimer(); // For this example, only initialize the ePWM Timers // Step 5. User specific code, enable interrupts: // Initialize counters: EPwm1TimerIntCount = 0; EPwm2TimerIntCount = 0; EPwm3TimerIntCount = 0; EPwm4TimerIntCount = 0; EPwm5TimerIntCount = 0; EPwm6TimerIntCount = 0; // Enable CPU INT3 which is connected to EPWM1-6 INT: IER |= M_INT3; // Enable EPWM INTn in the PIE: Group 3 interrupt 1-6 PieCtrlRegs.PIEIER3.bit.INTx1 = PWM1_INT_ENABLE; PieCtrlRegs.PIEIER3.bit.INTx2 = PWM2_INT_ENABLE; PieCtrlRegs.PIEIER3.bit.INTx3 = PWM3_INT_ENABLE; PieCtrlRegs.PIEIER3.bit.INTx4 = PWM4_INT_ENABLE; PieCtrlRegs.PIEIER3.bit.INTx5 = PWM5_INT_ENABLE; PieCtrlRegs.PIEIER3.bit.INTx6 = PWM6_INT_ENABLE; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Step 6. IDLE loop. Just sit and loop forever (optional): for(;;) { __asm(" NOP"); for(i=1;i<=10;i++) {} } } void InitEPwmTimer() { EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Stop all the TB clocks EDIS; // Setup Sync EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through EPwm6Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through // Allow each timer to be sync'ed EPwm1Regs.TBCTL.bit.PHSEN = TB_ENABLE; EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE; EPwm4Regs.TBCTL.bit.PHSEN = TB_ENABLE; EPwm5Regs.TBCTL.bit.PHSEN = TB_ENABLE; EPwm6Regs.TBCTL.bit.PHSEN = TB_ENABLE; EPwm1Regs.TBPHS.half.TBPHS = 100; EPwm2Regs.TBPHS.half.TBPHS = 200; EPwm3Regs.TBPHS.half.TBPHS = 300; EPwm4Regs.TBPHS.half.TBPHS = 400; EPwm5Regs.TBPHS.half.TBPHS = 500; EPwm6Regs.TBPHS.half.TBPHS = 600; EPwm1Regs.TBPRD = PWM1_TIMER_TBPRD; EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event EPwm1Regs.ETSEL.bit.INTEN = PWM1_INT_ENABLE; // Enable INT EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event EPwm2Regs.TBPRD = PWM2_TIMER_TBPRD; EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Enable INT on Zero event EPwm2Regs.ETSEL.bit.INTEN = PWM2_INT_ENABLE; // Enable INT EPwm2Regs.ETPS.bit.INTPRD = ET_2ND; // Generate INT on 2nd event EPwm3Regs.TBPRD = PWM3_TIMER_TBPRD; EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Enable INT on Zero event EPwm3Regs.ETSEL.bit.INTEN = PWM3_INT_ENABLE; // Enable INT EPwm3Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event EPwm4Regs.TBPRD = PWM4_TIMER_TBPRD; EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm4Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Enable INT on Zero event EPwm4Regs.ETSEL.bit.INTEN = PWM4_INT_ENABLE; // Enable INT EPwm4Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event EPwm5Regs.TBPRD = PWM5_TIMER_TBPRD; EPwm5Regs.TBCTL.bit.CTRMODE= TB_COUNT_UP; // Count up EPwm5Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Enable INT on Zero event EPwm5Regs.ETSEL.bit.INTEN = PWM5_INT_ENABLE; // Enable INT EPwm5Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event EPwm6Regs.TBPRD = PWM6_TIMER_TBPRD; EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm6Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Enable INT on Zero event EPwm6Regs.ETSEL.bit.INTEN = PWM6_INT_ENABLE; // Enable INT EPwm6Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Start all the timers synced EDIS; } // Interrupt routines uses in this example: __interrupt void epwm1_timer_isr(void) { EPwm1TimerIntCount++; // Clear INT flag for this timer EPwm1Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm2_timer_isr(void) { EPwm2TimerIntCount++; // Clear INT flag for this timer EPwm2Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm3_timer_isr(void) { EPwm3TimerIntCount++; // Clear INT flag for this timer EPwm3Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm4_timer_isr(void) { EPwm4TimerIntCount++; // Clear INT flag for this timer EPwm4Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm5_timer_isr(void) { EPwm5TimerIntCount++; // Clear INT flag for this timer EPwm5Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } __interrupt void epwm6_timer_isr(void) { EPwm6TimerIntCount++; // Clear INT flag for this timer EPwm6Regs.ETCLR.bit.INT = 1; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP3; } //=========================================================================== // No more. //===========================================================================
您现在是要实现什么功能?能否稍微描述下?您现在不需要使用计数器?
一般在程序内的用法如下
// Every 10'th interrupt, change the CMPA/CMPB values
if(epwm_info->EPwmTimerIntCount == 10)
用于中断计数,每多少次中断执行特定操作