This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D 4个ADC并行多次采集



想利用28377D 4个module中的4个ADC对四路信号并行采集。ADC配置需求如下:

1)4个module中的4个ADC对四路信号并行采集;

2)ADC开始采集时刻由GPIO输入外部触发信号;

3)四个ADC以大于4MSPS的速度连续采集四次,完成4次采集后停止采集,或者不在往缓存中写入新的数据。

请问怎么配置ADC和DSP内部存储器的关系,才能做到如上第3点?

第3点中提到的连续采集次数可以不是4次,只要≥3次即可。我是否可以让ADC讲采集数据存储在 DSP的ram中,而非register

  • 1、可以,因为每个ADC模块都有一个采样保持电路,可以保证4路同时采样
    2、ADC的采样触发条件中有GPIO: Input X-Bar INPUT5
    3、4MSPS是什么速度?F28377D的ADC每个转换器的吞吐量为3.5MSPS(系统吞吐量为 14MSPS)。“完成4次采集后停止采集”可以控制触发信号停止触发。
    “让ADC讲采集数据存储在 DSP的ram中,而非register”:寄存器的值也是在ram中的