This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28377 bootloader启动的问题



各位大侠:

         我最近在调试28277s,遇到一个问题,我按照SPRAAU8A的方法增加了BootLoader以后,在CCS6加载完成后没有跳转到main函数,而是停在0x03FE493处死循环。我的这个程序部用bootloader下调试是没有问题的,不用bootloader的方式直接在下载到flash运行也是没有问题。请各位帮帮我这是怎么回事?

code start文件内容如下:

WD_DISABLE .set 1                 ;set to 1 to disable WD, else set to 0

.ref copy_sections
.global code_start

***********************************************************************
* Function: codestart section
*
* Description: Branch to code starting point
***********************************************************************

.sect "codestart"

code_start:
.if WD_DISABLE == 1
LB wd_disable                   ;Branch to watchdog disable code
.else
LB copy_sections                 ;Branch to copy_sections
.endif

;end codestart section

***********************************************************************
* Function: wd_disable
*
* Description: Disables the watchdog timer
***********************************************************************
.if WD_DISABLE == 1

.text
wd_disable:
SETC OBJMODE             ;    Set OBJMODE for 28x object code
EALLOW                            ;           Enable EALLOW protected register access
MOVZ DP, #7029h>>6                ;              Set data page for WDCR register
MOV @7029h, #0068h         ;           Set WDDIS bit in WDCR to disable WD
EDIS                                           ;Disable EALLOW protected register access
LB copy_sections ;Branch to copy_sections

.endif

section copy内容如下:

.ref _c_int00
.global copy_sections
.global _cinit_loadstart, _cinit_runstart, _cinit_size
.global _const_loadstart, _const_runstart, _const_size
.global _econst_loadstart, _econst_runstart, _econst_size
.global _pinit_loadstart, _pinit_runstart, _pinit_size
.global _switch_loadstart, _switch_runstart, _switch_size
.global _text_loadstart, _text_runstart, _text_size

***********************************************************************
* Function: copy_sections
*
* Description: Copies initialized sections from flash to ram
***********************************************************************

.sect "copysections"

copy_sections:


MOVL XAR5,#_cinit_size                           ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_cinit_loadstart               ; Store Load Starting Address in XAR6
MOVL XAR7,#_cinit_runstart                    ; Store Run Address in XAR7
LCR copy                                                    ; Branch to Copy

MOVL XAR5,#_const_size                         ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_const_loadstart                ; Store Load Starting Address in XAR6
MOVL XAR7,#_const_runstart                 ; Store Run Address in XAR7
LCR copy                                                     ; Branch to Copy

MOVL XAR5,#_econst_size                     ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_econst_loadstart             ; Store Load Starting Address in XAR6
MOVL XAR7,#_econst_runstart               ; Store Run Address in XAR7
LCR copy                                                     ; Branch to Copy

MOVL XAR5,#_pinit_size                         ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_pinit_loadstart                 ; Store Load Starting Address in XAR6
MOVL XAR7,#_pinit_runstart                   ; Store Run Address in XAR7
LCR copy                                                       ; Branch to Copy

MOVL XAR5,#_switch_size                     ; Store Section Size in XAR5
MOVL ACC,@XAR5                                  ; Move Section Size to ACC
MOVL XAR6,#_switch_loadstart              ; Store Load Starting Address in XAR6
MOVL XAR7,#_switch_runstart               ; Store Run Address in XAR7
LCR copy                                                      ; Branch to Copy

MOVL XAR5,#_text_size                               ; Store Section Size in XAR5
MOVL ACC,@XAR5                                    ; Move Section Size to ACC
MOVL XAR6,#_text_loadstart                    ; Store Load Starting Address in XAR6
MOVL XAR7,#_text_runstart                     ; Store Run Address in XAR7
LCR copy                                                   ; Branch to Copy


LB _c_int00                                                 ; Branch to start of boot.asm in RTS library

copy:
B return,EQ                                                ; Return if ACC is Zero (No section to copy)

SUBB ACC,#1

RPT AL                                                        ; Copy Section From Load Address to
|| PWRITE *XAR7, *XAR6++                    ; Run Address

return:
LRETR                                                        ; Return

.end

CMD文件内容:


MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS : origin = 0x008000, length = 0x003000


RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE                  /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x07E000                 /* on-chip Flash */

PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

BOOT_RSVD : origin = 0x000002, length = 0x000120                     /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400                            /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800

RAMGS : origin = 0x00C000, length = 0x010000
}


SECTIONS
{
/* Allocate program areas: */

codestart : > BEGIN PAGE = 0, ALIGN(4)
copysections : > FLASHB PAGE = 0, ALIGN(4)

/*** Initialized Sections ***/
.cinit : LOAD = FLASHB, PAGE = 0            /* can be ROM */
RUN = RAMLS, PAGE = 0                          /* must be CSM secured RAM */
LOAD_START(_cinit_loadstart),
RUN_START(_cinit_runstart),
SIZE(_cinit_size)

.const : LOAD = FLASHB, PAGE = 0                 /* can be ROM */
RUN = RAMLS, PAGE = 0                              /* must be CSM secured RAM */
LOAD_START(_const_loadstart),
RUN_START(_const_runstart),
SIZE(_const_size)

.econst : LOAD = FLASHB, PAGE = 0                      /* can be ROM */
RUN = RAMLS, PAGE = 0                                      /* must be CSM secured RAM */
LOAD_START(_econst_loadstart),
RUN_START(_econst_runstart),
SIZE(_econst_size)

.pinit : LOAD = FLASHB, PAGE = 0                      /* can be ROM */
RUN = RAMLS, PAGE = 0                                         /* must be CSM secured RAM */
LOAD_START(_pinit_loadstart),
RUN_START(_pinit_runstart),
SIZE(_pinit_size)

.switch : LOAD = FLASHB, PAGE = 0                            /* can be ROM */
RUN = RAMLS, PAGE = 0                                            /* must be CSM secured RAM */
LOAD_START(_switch_loadstart),
RUN_START(_switch_runstart),
SIZE(_switch_size)

.text : LOAD = FLASHB, PAGE = 0                                   /* can be ROM */
RUN = RAMLS, PAGE = 0                                             /* must be CSM secured RAM */
LOAD_START(_text_loadstart),
RUN_START(_text_runstart),
SIZE(_text_size)


/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAMGS PAGE = 1
.esysmem : > RAMGS PAGE = 1

/* Initalized sections go in Flash */

.reset : > RESET, PAGE = 0, TYPE = DSECT                   /* not used, */

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/