This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前需要实现DSP28335和STM32F407的双机通信,DSP发送ARM接收,需要将407调至SPI的TI模式,自己根据参考手册将 SPI_CR2 寄存器中的 FRF 位置 1,以选择 TI 模式协议进行串行通信,arm的spi配置程序如下
void SPI2_Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
SPI_InitTypeDef SPI_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB|RCC_AHB1Periph_GPIOC, ENABLE); //使能GPIOB时钟
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); //使能SPI2时钟
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; //复用功能
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; //推挽输出
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; //100MHz
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; //上拉
GPIO_Init(GPIOB, &GPIO_InitStructure); //初始化IO口
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; //复用功能
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; //推挽输出
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; //100MHz
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2|GPIO_Pin_3;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource13,GPIO_AF_SPI2); //PB13复用为 SPI2
GPIO_PinAFConfig(GPIOC,GPIO_PinSource2,GPIO_AF_SPI2); //PC2复用为 SPI2
GPIO_PinAFConfig(GPIOC,GPIO_PinSource3,GPIO_AF_SPI2); //PC3复用为 SPI2
GPIO_PinAFConfig(GPIOB,GPIO_PinSource12,GPIO_AF_SPI2); //PB12复用为 SPI2
GPIO_ResetBits(GPIOB,GPIO_Pin_13); //PB13上拉
GPIO_SetBits(GPIOC,GPIO_Pin_2|GPIO_Pin_3); //PC2/3上拉
GPIO_SetBits(GPIOB,GPIO_Pin_12); //PB12上拉
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; //设置SPI单向或者双向的数据模式:SPI设置为双线双向全双工
SPI_InitStructure.SPI_Mode = SPI_Mode_Slave; //设置SPI工作模式:设置为主SPI
SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; //设置SPI的数据大小:SPI发送接收16位帧结构
//SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; //选择了串行时钟的稳态:时钟悬空低
//SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; //数据捕获于第二个时钟沿 下降沿有效
SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; //NSS信号由硬件(NSS管脚)还是软件(使用SSI位)管理:内部NSS信号有SSI位控制
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; //定义波特率预分频的值:波特率预分频值为256
//SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; //指定数据传输从MSB位还是LSB位开始:数据传输从MSB位开始
SPI_InitStructure.SPI_CRCPolynomial = 7; //CRC值计算的多项式
SPI_Init(SPI2, &SPI_InitStructure); //根据SPI_InitStruct中指定的参数初始化外设SPIx寄存器
SPI2->CR2|= 0x0010; // SPI TI模式
SPI_Cmd(SPI2, ENABLE); //使能SPI外设
SPI_I2S_ITConfig(SPI2,SPI_I2S_IT_RXNE,ENABLE); //中断开启函数
//SPI2_ReadWriteByte(0xff);//启动传输
}
但实验时,arm无法接收到程序,DSP发送数据波形与下图一致,想要一份arm TI模式的例程,谢谢