This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D EtherCAT 在EMIF2模式下调试失败

hi all;

     最近调试28379D EtherCAD 使用ControlSuite 中TMDSECATCND379D_V1.0中的例程,SPI接口下能正常进入OP模式,但是在EMIF2接口下就只能在运行在INIT模式下,有哪位遇到类似问题吗,请帮忙解惑一下,万分感谢!

    我用的硬件是:http://www.ti.com/tool/TMDSECATCNCD379D

                             http://www.ti.com.cn/tool/cn/tmdxiddk379d

  • 您可以看一下 内的相关说明

    In the TMDSECATCNCD379D design, the F2837x receives EtherCAT data from the ET1100 through either a serial (SPI) interface or an asynchronous parallel memory interface (EMIF). Figure 7 shows the use of EMIF2, but either EMIF can be used to interface to the ET1100. Note that GPIOs 93 and 94 are for future expansion to address a larger memory space. They are not used in the example code

  • Hi,能否提供一个在TMDSECATCNCD379D模块上运行的包含SDO输入输出的例程来参考一下呢?