This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何将28377D的ADC采样率达到最高



由于需要用到数据采集,不得已挖掘下这块芯片的ADC潜能

看了官方文件,在200M系统时钟时,采样保持15个系统时钟周期,转换时间43个系统时钟周期,算下来采样一次用时290ns,不停采集的话差不多3.448M

使用场景是收到外部触发脉冲后就AD采集并记录,

我使用ecap捕获脉冲,在ecap的中断中,软件置位开始采集(AdcaRegs.ADCSOCFRC1.all = 0x0001; ),然后采集转换完成后触发ADC中断,在ADC中断中记录采集到的数据

本以为这么高弄个2M不成问题,结果实际只能到900K,1M频率时就开始漏采集数据了。

另:漏采集数据的个人判断方法为,在ecap中断与ADC中断中各设一个静态变量从开始累加计数,每进一次中断就加1,触发频率900K一下,两个计数器数值一致,但从1M频率开始就有差异了,1.2M时差异就大的分不出到底漏采集了多少数据了……

  • 串行处理器 执行加上中断 耗周期比较多
  • 您可以看一下下面的帖子给出的详细回复

    e2e.ti.com/.../584025

    The ADC conversion time is given in table Table 5-51. "ADC Timings in 12-Bit Mode (SYSCLK Cycles)". From this table, the conversion time when the ADC is operating /4 of the SYSCLK (typical when the CPU is running at 200MHz) would be 44 cycles. The minimum S+H is 75ns @ 200MHz = 15 cycles. Total ADC time between samples therefore needs to be at least 59 cycles. If you want 10MSPS then a sample has to occur every 20 cycles. With 4 ADCs each ADC samples once every 80 cycles, which is > than 59, so possible.

    To generate the triggers, you will probably want to use 2 synchronized ePWMs, each with a period of 80 cycles. Each ePWM can generate triggers for two of the ADCs.

    As far as memory, 10MSPS * 0.25 seconds = 2.5M samples. Each sample is 12-bit, so they take up a full 16-bit word. There is as much as 106K x 16 on-chip RAM, so you are definitely going to need an external memory connected to the EMIF peripheral. It should be possible for the DMA to move ADC samples to the EMIF, and for the EMIF to write to external memory without CPU intervention.

    As far as performance, take a look at the ENOB section in the datasheet table "ADC Characteristics (12-Bit Single-Ended Mode)". In this interleaved cases, the ADCs are not operating in lock-step, so we have to consider the "Asynchronous ADCs" performance specification. For the ZWT package (BGA) this is 10.9 bits and for the PTP pacakge (QFP) this is 9.7 bits. Both should be OK, but note that the single-core F28377x launchpad uses the PZP package, which has bad enough performance in this case that it is "not supported". The PZP package also only has 2 ADCs pinned-out, so you probably would want to get the F283779D dual-core launchpad if you want to use a launchpad as your development platform for this.

    In addition to the non-lockstep performance penalty, interleaving ADCs will give you some very significant tones due to ADC-to-ADC gain, offset, and linearity mismatch. We specify the ADC-to-ADC gain and offset error in the datasheet as +/-4 LSBs and +/-2 LSBs (both typical), so I think you should probably be OK to meet 8-bits of performance.
  • 非常感谢,虽然与触发采样情况不一样,但启发了不少
  • 很高兴能帮到您