目前在公司预研的转台中,遇到的问题是,DSP28335连接4个Ad2s1210和两个ADS8588。
连接4个AD2S1210,是因为有两个轴向,一个高低轴向和一个方位轴向。旋变是多级旋变,有粗机和精机之分,有两组激磁和两组正余弦信号,每个轴向两个AD2S1210。因此项目中需要用4个AD2S1210。通过外扩总线与DSP28335连接。
而ADS8588采集两个轴向的相电压和相电流,所以需要两个ADS8588。通过外扩总线与DSP28335连接。
我的问题是DSP28335外扩总线(XINTF)可以驱动多少个门电路,外扩这六个片子在不加总线驱动器的情况下,会不会有驱动能力不够的情况。