This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问F28377D的HRPWM模块是否支持 高精度周期和高精度死区同时运行?



请问F28377D的HRPWM模块是否支持 高精度周期和高精度死区同时运行?      就是是否可以同时配置成高精度周期和高精度死区

  • 所谓HR是High Resolution的缩写,即高分辨率,刚看了一下TI的官方资料,高分辨率技术是通过一种叫做微边沿定位器(micro edge positioner (MEP))的技术来实现在相同系统时钟的情况下把PWM的分辨率提高,TI给的资料里介绍此技术是相当于把计数器时钟提高80倍而提到的,TI给出的数据如下:在100MHz系统时钟的情况下,如果想要输出200KHz的PWM信号,普通PWM发生器只能提供9位的分辨率,而使用HRPWM技术可以在输出200KHz的PWM信号情况下提供14.8位的分辨率,所以HR技术就是在于提高PWM信号的有效分辨率。所以对于产生正弦波的情况下当然最好是用HRPWM,因为在相同分辨率的情况下,HRPWM可以产生更高的频率。不过一般产生正弦波输出都是需要加滤波器的。
    计数器精度提高了 周期 死区都会提高
  • F2837X是可以输出成对带死区的高精度PWM的