This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2812例程BLDC3-1的一个疑惑



例程倒数第二个语句:

// Note: To be safe, use a mask value to write to the entire
 // EVAIFRB register.  Writing to one bit will cause a read-modify-write
 // operation that may have the result of writing 1's to clear
 // bits other then those intended.
    EvaRegs.EVAIFRB.all = BIT0;

说是为了保证系统安全工作,屏蔽定时器T2,‘

我的问题是为什么要屏蔽呢,屏蔽了不是不能中断了吗

  • 请您在提问时给出具体的例程,BLDC3-1的例程还是很多的。只给出一段代码,我也记不住是具体哪个例程
  • // ***************** LEVEL3 *****************
    #if (BUILDLEVEL==LEVEL3)
    // ------------------------------------------------------------------------------
    //    Call the ADC04U_DRV read function.
    // ------------------------------------------------------------------------------
       adc1.read(&adc1);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the RMP module and call the Ramp control
    //    calculation function.
    // ------------------------------------------------------------------------------
          rc1.TargetValue = _IQ(SpeedRef);
          rc1.calc(&rc1);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the HALL module and call the Hall sensor
    //    read function.
    // ------------------------------------------------------------------------------
          hall1.HallMapPointer = (int16)mod1.Counter;
          hall1.read(&hall1);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the MOD6 module and call the Modulo 6 counter
    //    calculation function.
    // ------------------------------------------------------------------------------
          mod1.TrigInput =(int32)hall1.CmtnTrigHall;
          mod1.Counter = (int32)hall1.HallMapPointer;
          mod1.calc(&mod1);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the RMP2 module and call the Ramp control 2
    //    calculation function.
    // ------------------------------------------------------------------------------
          rmp2.DesiredInput = (int32)DFuncDesired;
          rmp2.calc(&rmp2);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the PID_REG3 module and call the PID speed controller
    //    calculation function.
    // ------------------------------------------------------------------------------ 
          pid1_spd.Ref = rc1.SetpointValue;
          pid1_spd.Fdb = speed1.Speed;
          pid1_spd.calc(&pid1_spd);
    // ------------------------------------------------------------------------------
    //    Set the speed closed loop flag once the speed is built up to a desired value.
    // ------------------------------------------------------------------------------
          if (rc1.EqualFlag == 0x7FFFFFFF)  {
             SpeedLoopFlag = TRUE;
             rc1.RampDelayMax = 300; 
          }
    // ------------------------------------------------------------------------------
    //    Connect inputs of the PWM_DRV module and call the PWM signal generation
    //    update function.
    // ------------------------------------------------------------------------------
       // Switch from fixed duty-cycle or controlled Speed duty-cycle by SpeedLoopFlag variable
          if (SpeedLoopFlag == FALSE)
             pwm1.DutyFunc = (int16)rmp2.Out;           // fixed duty-cycle
          else
             pwm1.DutyFunc = (int16)_IQtoIQ15(pid1_spd.Out);   // controlled Speed duty-cycle
          pwm1.CmtnPointer = (int16)mod1.Counter;
          pwm1.update(&pwm1);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the SPEED_PR module and call the speed calculation
    //    function.
    // ------------------------------------------------------------------------------ 
          if ((mod1.Counter == 5)&(hall1.CmtnTrigHall == 0x7FFF)) {
             speed1.TimeStamp = VirtualTimer;
             speed1.calc(speed1);
          }
    // ------------------------------------------------------------------------------
    //    Connect inputs of the DATALOG module
    // ------------------------------------------------------------------------------
          DlogCh1 = (int16)mod1.Counter;
          DlogCh2 = (int16)mod1.TrigInput;
          DlogCh3 = (int16)_IQtoIQ15(pid1_spd.Ref);
          DlogCh4 = (int16)_IQtoIQ15(pid1_spd.Fdb);
    // ------------------------------------------------------------------------------
    //    Connect inputs of the EN_DRV module and call the enable/disable PWM signal
    //    update function (for DMC1500 only).
    // ------------------------------------------------------------------------------   
          drv1.EnableFlag = EnableFlag;
          drv1.update(&drv1);
    #endif // (BUILDLEVEL==LEVEL3)

    // ------------------------------------------------------------------------------
    //    Increase virtual timer and force 15 bit wrap around
    // ------------------------------------------------------------------------------
     VirtualTimer++;
     VirtualTimer &= 0x00007FFF;
    // ------------------------------------------------------------------------------
    //    Call the DATALOG update function.
    // ------------------------------------------------------------------------------
        dlog.update(&dlog);

    #if (DSP_TARGET==F2808)
    // Acknowledge interrupt to recieve more interrupts from PIE group 1
     PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
    #endif

    #if (DSP_TARGET==F2812)
    // Enable more interrupts from this timer
     EvaRegs.EVAIMRB.bit.T2PINT = 1;
     
    // Note: To be safe, use a mask value to write to the entire
     // EVAIFRB register.  Writing to one bit will cause a read-modify-write
     // operation that may have the result of writing 1's to clear
     // bits other then those intended.
        EvaRegs.EVAIFRB.all = BIT0;*************************************就是这句********************************
     
    // Acknowledge interrupt to recieve more interrupts from PIE group 3
     PieCtrlRegs.PIEACK.all |= PIEACK_GROUP3;
    #endif
    }
    您好,感谢您的回答,我有疑问的那句就在这段的倒数第6行
  • 您可以看一下TRM内的说明

    Since EVxIFRx are readable registers, occurrence of an interrupt event can be monitored by software polling the appropriate bit in EVxIFRx when the interrupt is masked.