This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28375s HTQFP (PZP)100引脚封装用Ultra librarian导出AD文件空白



28375s HTQFP (PZP)100引脚封装用Ultra librarian导出AD文件空白,谁有2837x 系列100引脚的分装,急用,十分感谢~

  • 你好,请问你使用的是以下主页提供的封装文件吗?
    www.ti.com.cn/.../pinout-quality
  • 是的,试了好多遍都不行,之前转过别的封装都可以
  • 你好,我这边按照官网的说明步骤是可以打开的。你是直接在页面上下载的软件吗?

  • 我这个也能打开,只是转化完用ad打开后空白

  • 您好! 您可以帮忙转成AD的封装么,我转了几次打开都是空白,谢谢!

  • 你好,你这边方便提供一下使用的软件型号、版本,以及打开出现错误的截图吗?我去咨询一下美国方面的相关人员
  • # Created by Ultra Librarian Lite 8.1.204 Copyright ? 1999-2016
    # Ultra Librarian Free Reader, Accelerated-Designs Inc.
    
    StartFootprints
    EndFootprints
    
    StartComponents
    EndComponents
    
    Ultra librarian版本8.1.204

    导入到AD16后空白

    附件是导出时生成的文件

     
     
     
    **********************************************************
    *************  Important Instructions Follow  ************
    **********************************************************
     
    All files exported to: C:\UltraLibrarian\Library\Exported\Altium\2019-05-25_11-36-49\2019-05-25_11-36-49
     
     
    To import your new library part into Altium follow these steps:
    
    1. After running the Ultra Librarian export for the first time,
    you will need to copy the following files into an area where
    they can be accessed for all future translations.  They are script
    files that Altium will need to be able to find.
    	a. UL_Form.dfm
    	b. UL_Form.pas
    	c. UL_Import.pas
    	d. UL_Import.prjScr
    	
    2. The above script file will need to be run from within Altium.
    This can be done by going to File, Open and selecting the
    UL_Import.PrjScr file stored above.
    
    3. Select the UL_Form.pas file form the new project that has loaded,
    and then select runfrom the drop down menu.  You will need to select
    the form again. Run the form.
    
    3. When the script is run, it will ask you for the file name of the
    Ultra Librarian file to run.  You should select the latest file
    produced with a date code (for instance 2010-02-17_23-12-34.txt).
    
    4. The script will open a new Integraged Library project and import
    the Ultra Librarian data into it.  When complete a message box
    will pop up saying that import is done.
    
    For additional information, please visit this site:
    http://www.accelerated-designs.com/help/Altium_import.html
    
    For a video tutorial, please visit:
    http://youtu.be/pih50yx9HYU
     
     
    Padstack "RX10p63Y57p53D0T_1" renamed to "RX10p63Y57p53D0T"
    Padstack "RX340p16Y340p16D0T_1" renamed to "RX340p16Y340p16D"
    Symbol "TMS320F28375S_PZP_100_01" renamed to "TMS320F28375S_PZ"
    Symbol "TMS320F28375S_PZP_100_00" renamed to "TMS320F28375S_00"
    Symbol "TMS320F28375S_PZP_100" renamed to "TMS320F28375S_01"
    Symbol "TMS320F28375S_PZP_100_01_1" renamed to "TMS320F28375S_02"
    Symbol "TMS320F28375S_PZP_100_A" renamed to "TMS320F28375S_03"
    Symbol "TMS320F28375S_PZP_100_B" renamed to "TMS320F28375S_04"
    Component "TMS320F28375S_PZP_100" renamed to "TMS320F28375S_PZ"
    
    
    Ultra Librarian Lite 8.1.204 Process Report
    
    
    Message - Pattern "PZP-100", entity (1286-Line) is a LINE with matching start and end points.
    Message - Pattern "PZP-100", entity (1288-Line) is a LINE with matching start and end points.
    Message - Pattern "PZP-100", entity (1290-Line) is a LINE with matching start and end points.
    Message - Pattern "PZP-100", entity (1292-Line) is a LINE with matching start and end points.
    
    TextStyle count:  69
    Padstack count:   3
    Pattern count:    1
    Symbol count:     6
    Component count:  1
    
    Export
    
    Pad style "RX340p16Y340p16D" is a complex style and will be skipped.
    Footprint "PZP-100" requires pad style "RX340p16Y340p16D" and will be skipped.
    Component "TMS320F28375S_PZ" requires footprint "PZP-100" and will be skipped.
    Pad style "EX20Y20D10P_1" is a complex style and will be skipped.
    

  • 你好,美国方面已经确认文件有问题,但需要开发团队修复,有消息了会联系你。
  • 你好,查看一下附件的文件是否有用。0116.soprano_176_in_pkg_handoff_revb.zip

  • 您好 我下载了您发给我的连接,但是.bsd格式的文件不知道怎么打开,用Ultra Librarian不能导入该格式文件,谢谢!

  • 你好,如果可以使用的话给一个反馈,谢谢
  • 我试了 打开还是空白
  • 你好,对方团队跟我确认了一下文件没问题,可以用Ultralibriarian打开为Altium文件。你这边方便提供一下你的操作步骤以及对于的信息截图吗?
  • 你好,这是另一个版本,尝试一下

    TMS320F28375S_PZP_100.zip

  • 这个可以,十分感谢!