This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的matlab底层支持包可靠性怎么样?



最近要做一个28335的项目,想尝试用matlab的C2000底层包直接生成底层代码,但是不知道这个可靠性怎么样,28335这款芯片也已经出现很多年了,matlab的底层包是不是也已经很完善了,会不会出问题?

希望有大师解答一下,给个建议,感激不尽!

  • 你好,用matlab的C2000底层包直接生成底层代码应该已经是很成熟的一项功能了。至于你说的会不会出问题,主要还是看你对产品的熟悉度。因为两款的产品的应用在当下已经处于非常成熟的地步了
  • 您好,谢谢您的答复,另外还有几个问题:
    1、simulink生成的c2000底层代码是否为商业级可以直接做产品的?我这边弄了个简单的模型生成了一下,发现所能看到的代码行数一个模块可能只有两百多行,比如发送失败、写失败都有没有做相应的考虑,这个代码是否成熟呢?
    2、我们这边最终是想实现CAN烧录功能的,如果用这个底层包直接生成的话可以实现吗,有Bootloader相关内容吗?

    不好意思,问题有点多......能否再解答一下~
  • 这两个问题可能都需要你去咨询simulink的技术支持,目前常见的CAN烧录都是在CCS上直接转成.hex文件进行烧写,没经过simulink,不确定能否实现。或者你也可以去我们英文论坛咨询一下美国工程师这方面的问题:e2e.ti.com/.../171
  • 完全没问题的,之前我们用28335做过模型设计,现在也一直在用28377D做模型设计,都能正常应用到产品上的。