This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28379D 为什么将ePWM触发模式由上升下降沿改为上升沿或者下降沿之后pwm无输出信号?



当我将epwm的计数模式从上升下降沿改为下降沿或者上升沿之后模块无PWM输出信号,通过JTAG在线调试发现CMPA或者CMPB寄存器都有值,可为什么没有输出呢?

EPwm2Regs.TBPRD = (Uint16)(TLBDC_PER); //PWM period
EPwm2Regs.TBPHS.bit.TBPHS = 0;//TLBDC_PHASE(120.0f);//0; //No phase shift
EPwm2Regs.TBCTL.bit.FREE_SOFT = 2; //Free run
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; //System clock out / 1
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; //System clock out / 1
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;//TB_SYNC_IN;//TB_CTR_ZERO; //Send synchronization signal when counter = 0
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW; //Using shadow register for PWM period
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;//TB_DISABLE; //Master, don't need load phase register
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN;//TB_COUNT_UPDOWN; //TB_COUNT_UP;//Up-down mode

/* Counter compare register initialization */
EPwm2Regs.CMPA.bit.CMPA = TLBDC_CMPA(0);//TLBDC_CMPA(0.3);//cmpa=zkb*prd(s1),zkb=pi_out
EPwm2Regs.CMPB.bit.CMPB = TLBDC_CMPB(0);//TLBDC_CMPB(0.3);//phase=180; zkb'=pi_out,cmpb=(1-zkb')*prd=(1-pi_out)*prd (s2,pass a not logic->s3)
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;//Using shadow register for compare
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;//Using shadow register for compare
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;//Load new compare value when counter = period
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;//CC_CTR_ZERO;//Load new compare value when counter = zero

EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR;//Set PWM to low when counter increase and = compare A
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET;//Set PWM to high when counter decrease and = compare A
EPwm2Regs.AQCTLB.bit.CBU = AQ_SET;//Set PWM to low when counter increase and = compare A
EPwm2Regs.AQCTLB.bit.CBD = AQ_CLEAR;//Set PWM to high when counter decrease and = compare A

EPwm2Regs.DBCTL.bit.IN_MODE = DBB_RED_DBA_FED;//DBA_RED_DBB_FED;//s5=1,s4=0
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;//DBB_ENABLE;//DB_DISABLE;//DBB_ENABLE;// s1=0,s0=1(Q3)->0(Q2)
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HI;//DB_ACTV_LO;//0x00;//DB_ACTV_HIC;// s3=1,s2=0->1, Active Hi complementary
EPwm2Regs.DBFED = 0x00;//INV_DEAD_CYCLE;// FED = INV_DEAD_CYCLE TBCLKs
EPwm2Regs.DBRED = 0;//INV_DEAD_CYCLE;// RED = INV_DEAD_CYCLE TBCLKs
EPwm2Regs.DBCTL.bit.OUTSWAP = 0x03;

//add soca
EPwm2Regs.ETSEL.bit.SOCAEN=ET_ENABLE;//enable
EPwm2Regs.ETSEL.bit.SOCASEL=ET_CTR_PRDZERO;//ET_CTR_PRDZERO;
EPwm2Regs.ETPS.bit.SOCAPRD=ET_1ST;//divide frequency, page69/117.

//1 1 2 3-Generate the EPWMxSOCA pulse on the first second third event:
//2 Once the SOCA pulse is generated, the ETPS[SOCACNT] bits will automatically be cleared.
EPwm2Regs.ETSEL.bit.SOCBEN=ET_ENABLE;//enable
EPwm2Regs.ETSEL.bit.SOCBSEL=ET_CTR_PRDZERO;//ET_CTR_ZERO;
EPwm2Regs.ETPS.bit.SOCBPRD=ET_1ST;//divide frequency
//3 Generate the EPWMxSOCA pulse on the first event: ETPS[SOCACNT] = 0,1
EPwm2Regs.ETSEL.bit.INTEN=ET_DISABLE;
EPwm2Regs.ETPS.bit.INTPRD=ET_DISABLE;

  • 你好,你原始的程序中使用递增递减计数模式,那么你的比较器在计数器递增递减的过程中会各自触发一次上升或者下降动作(如递增的时候到达CMPA值触发PWMA高电平,递减的时候到达CMPA值触发PWMA低电平),形成一个完整的PWMA波形。
    但是一旦将计数模式改为递增或者递减模式,那么你原先配置的触发动作只会执行一次。即,要么只在递增模式的时候触发CMPA值触发PWMA高电平,要么递减的时候到达CMPA值触发PWMA低电平。PWM的输出只会是永远为“高”或者永远为“低”
    所以,如果要将计数模式从递增递减模式改为递增或者递减模式的话,需要更改对应CMPA、CMPB事件的动作才能输出完整的PWM波形。
    而将计数模式从递增改为递减,或者递减改为递增,那么只会使PWM输出相反的波形。