TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的EPWM丢失现象

我在使用28335配置一个变周期和变占空比的程序时,想要实现每次计数值等于周期值时进入EPWM中断,给周期值和比较值进行赋值,从而在一个循环计数中,不断改变周期和占空比。现在是想要实现12个脉冲周期一个循环变时,出现有一个周期占空比丢失的情况,实际测量发现该次是进入中断,并且进行了计数,但是没有进行比较操作,也就是这个周期内全为低电平,之后正常进入下一个周期。请问这个可能是什么原因导致的?图中示波器波形是,1.使用一个GPIO引脚电平变化测试中断执行时间波形,进入电平为1,退出变成0 2.EPWM波形。

这是EPWM1中断函数配置:

interrupt void epwm1_isr(void)
{
   // Update the CMPA and CMPB values
       GpioDataRegs.GPASET.bit.GPIO6 = 1;
      
   
                 flag_in=1;
        i++;
        if(i>=13)
        {
         i=1;
        }
        if(flag_in==1)
        {
         switch(i)
              {
              case 1:EPwm1Regs.TBPRD=173;
                     EPwm1Regs.CMPA.half.CMPA=130;
                    flag_in=0;

                    break;
              case 2:EPwm1Regs.TBPRD=393;
                     EPwm1Regs.CMPA.half.CMPA=267;
                     flag_in=0;
                     break;
              case 3:EPwm1Regs.TBPRD=373;
                     EPwm1Regs.CMPA.half.CMPA=178;
                     flag_in=0;
                     break;
              case 4:EPwm1Regs.TBPRD=323;
                     EPwm1Regs.CMPA.half.CMPA=107;
                     flag_in=0;
                     break;
             
              case 5:EPwm1Regs.TBPRD=251;
                     EPwm1Regs.CMPA.half.CMPA=50;
                     flag_in=0;
                     break;
             
              case 6:EPwm1Regs.TBPRD=337;
                     EPwm1Regs.CMPA.half.CMPA=37;
                     flag_in=0;
                     break;
                    
              case 7:EPwm1Regs.TBPRD=336;
                     EPwm1Regs.CMPA.half.CMPA=36;
                     flag_in=0;
                     break;
                   
              case 8:EPwm1Regs.TBPRD=237;
                     EPwm1Regs.CMPA.half.CMPA=37;
                     flag_in=0;
                     break;
                    
              case 9:EPwm1Regs.TBPRD=266;
                     EPwm1Regs.CMPA.half.CMPA=50;
                     flag_in=0;
                     break;
                    
              case 10:EPwm1Regs.TBPRD=302;
                     EPwm1Regs.CMPA.half.CMPA=107;
                     flag_in=0;
                     break;
                    
              case 11:EPwm1Regs.TBPRD=304;
                     EPwm1Regs.CMPA.half.CMPA=178;
                     flag_in=0;
                     t++;
                     break;
                 
              case 12:EPwm1Regs.TBPRD=311;
                     EPwm1Regs.CMPA.half.CMPA=267;
                     flag_in=0;
                                     
                     break;
             
//              case 13:EPwm1Regs.TBPRD=311;
//                     EPwm1Regs.CMPA.half.CMPA=267;
//                     flag_in=0;
//
//                     break;
             
              }

        }
  GpioDataRegs.GPACLEAR.bit.GPIO6 = 1;
      // Clear INT flag for this timer
    
         EPwm1Regs.ETCLR.bit.INT = 1;
         // Acknowledge this interrupt to receive more interrupts from group 3
         PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
这是EPWM配置:
InitEPwm1Gpio();
 InitEPwm2Gpio();
 InitEPwm3Gpio();
 InitEPwm4Gpio();
 InitEPwm5Gpio();
 InitEPwm6Gpio();
// EPwm1Regs.TBSTS.all=0;
// EPwm2Regs.TBSTS.all=0;
// EPwm3Regs.TBSTS.all=0;
// EPwm4Regs.TBSTS.all=0;
 EPwm1Regs.TBPHS.half.TBPHS=0;
 EPwm2Regs.TBPHS.half.TBPHS=0;
 EPwm3Regs.TBPHS.half.TBPHS=0;
 EPwm4Regs.TBPHS.half.TBPHS=0;
    EPwm5Regs.TBPHS.half.TBPHS=0;
 EPwm6Regs.TBPHS.half.TBPHS=0;
 
 EPwm1Regs.TBCTR=0;
 EPwm2Regs.TBCTR=0;
 EPwm3Regs.TBCTR=0;
 EPwm4Regs.TBCTR=0;
 EPwm5Regs.TBCTR=0;
 EPwm6Regs.TBCTR=0;
// EPwm1Regs.CMPCTL.all=0x00;        // Shadow mode for CMPA and CMPB
// EPwm2Regs.CMPCTL.all=0x00;
// EPwm3Regs.CMPCTL.all=0x00;
// EPwm4Regs.CMPCTL.all=0x00;
    EPwm1Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.SHDWBMODE=CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.LOADAMODE=CC_CTR_ZERO;
    EPwm1Regs.CMPCTL.bit.LOADBMODE=CC_CTR_ZERO;
    EPwm2Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.SHDWBMODE=CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.LOADAMODE=CC_CTR_ZERO;
    EPwm2Regs.CMPCTL.bit.LOADBMODE=CC_CTR_ZERO;
    EPwm3Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.SHDWBMODE=CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.LOADAMODE=CC_CTR_ZERO;
    EPwm3Regs.CMPCTL.bit.LOADBMODE=CC_CTR_ZERO;
    EPwm4Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW;
    EPwm4Regs.CMPCTL.bit.SHDWBMODE=CC_SHADOW;
    EPwm4Regs.CMPCTL.bit.LOADAMODE=CC_CTR_ZERO;
    EPwm4Regs.CMPCTL.bit.LOADBMODE=CC_CTR_ZERO;
    EPwm5Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW;
    EPwm5Regs.CMPCTL.bit.SHDWBMODE=CC_SHADOW;
    EPwm5Regs.CMPCTL.bit.LOADAMODE=CC_CTR_ZERO;
    EPwm5Regs.CMPCTL.bit.LOADBMODE=CC_CTR_ZERO;
    EPwm6Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW;
    EPwm6Regs.CMPCTL.bit.SHDWBMODE=CC_SHADOW;
    EPwm6Regs.CMPCTL.bit.LOADAMODE=CC_CTR_ZERO;
    EPwm6Regs.CMPCTL.bit.LOADBMODE=CC_CTR_ZERO;
// EPwm1Regs.AQCTLA.all=0x61;        // EPWMxA = 1 when CTR=CMPA and counter inc
// EPwm2Regs.AQCTLA.all=0x61;
// EPwm3Regs.AQCTLA.all=0x61;
// EPwm4Regs.AQCTLA.all=0x61;
    EPwm1Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm1Regs.AQCTLA.bit.PRD=AQ_CLEAR;
    EPwm2Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm2Regs.AQCTLA.bit.PRD=AQ_CLEAR;
    EPwm3Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm3Regs.AQCTLA.bit.PRD=AQ_CLEAR;
    EPwm4Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm4Regs.AQCTLA.bit.CAD=AQ_CLEAR;
    EPwm5Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm5Regs.AQCTLA.bit.CAD=AQ_CLEAR;
    EPwm6Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm6Regs.AQCTLA.bit.CAD=AQ_CLEAR;
// EPwm1Regs.AQCTLB.all=0x92;
// EPwm2Regs.AQCTLB.all=0x92;
// EPwm3Regs.AQCTLB.all=0x92;
// EPwm4Regs.AQCTLB.all=0x601;
// EPwm1Regs.AQSFRC.all=0;
// EPwm1Regs.AQCSFRC.all=0;
// EPwm2Regs.AQSFRC.all=0;
// EPwm2Regs.AQCSFRC.all=0;
// EPwm3Regs.AQSFRC.all=0;
// EPwm3Regs.AQCSFRC.all=0;
// EPwm4Regs.AQSFRC.all=0;
//  EPwm4Regs.AQCSFRC.all=0;
 
 EPwm1Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE;       
 EPwm1Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC;
 EPwm1Regs.DBCTL.bit.IN_MODE=DBA_ALL;
 EPwm1Regs.DBRED=Dead_time;
 EPwm1Regs.DBFED=Dead_time;
 EPwm2Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE;       
 EPwm2Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC;
 EPwm2Regs.DBCTL.bit.IN_MODE=DBA_ALL;
 EPwm2Regs.DBRED=Dead_time;
 EPwm2Regs.DBFED=Dead_time;
 EPwm3Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE;       
 EPwm3Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC;
 EPwm3Regs.DBCTL.bit.IN_MODE=DBA_ALL;
 EPwm3Regs.DBRED=Dead_time;
 EPwm3Regs.DBFED=Dead_time; 
 EPwm4Regs.DBCTL.bit.OUT_MODE=DB_DISABLE;  //不设置死区     
 EPwm4Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC;
 EPwm4Regs.DBCTL.bit.IN_MODE=DBA_ALL;
 EPwm4Regs.DBRED=Dead_time;//3us
 EPwm4Regs.DBFED=Dead_time; 
    EPwm5Regs.DBCTL.bit.OUT_MODE=DB_DISABLE;  //不设置死区     
 EPwm5Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC;
 EPwm5Regs.DBCTL.bit.IN_MODE=DBA_ALL;
 EPwm5Regs.DBRED=Dead_time;//3us
 EPwm5Regs.DBFED=Dead_time; 
 EPwm6Regs.DBCTL.bit.OUT_MODE=DB_DISABLE;  //不设置死区     
 EPwm6Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC;
 EPwm6Regs.DBCTL.bit.IN_MODE=DBA_ALL;
 EPwm6Regs.DBRED=Dead_time;//3us
 EPwm6Regs.DBFED=Dead_time; 
 
 
 EPwm1Regs.TZSEL.all=0;
 EPwm2Regs.TZSEL.all=0;
 EPwm3Regs.TZSEL.all=0;
 EPwm4Regs.TZSEL.all=0;
 EPwm5Regs.TZSEL.all=0;
 EPwm6Regs.TZSEL.all=0;
 EPwm1Regs.TZCTL.all=0;
 EPwm2Regs.TZCTL.all=0;
 EPwm3Regs.TZCTL.all=0;
 EPwm4Regs.TZCTL.all=0;
 EPwm5Regs.TZCTL.all=0;
 EPwm6Regs.TZCTL.all=0;
 EPwm1Regs.TZEINT.all=0;
 EPwm2Regs.TZEINT.all=0;
 EPwm3Regs.TZEINT.all=0;
 EPwm4Regs.TZEINT.all=0;
 EPwm5Regs.TZEINT.all=0;
 EPwm6Regs.TZEINT.all=0;
 EPwm1Regs.TZFLG.all=0;
 EPwm2Regs.TZFLG.all=0;
 EPwm3Regs.TZFLG.all=0;
 EPwm4Regs.TZFLG.all=0;
 EPwm5Regs.TZFLG.all=0;
 EPwm6Regs.TZFLG.all=0;
 EPwm1Regs.TZCLR.all=0;
 EPwm2Regs.TZCLR.all=0;
 EPwm3Regs.TZCLR.all=0;
 EPwm4Regs.TZCLR.all=0;
 EPwm5Regs.TZCLR.all=0;
 EPwm6Regs.TZCLR.all=0;
 EPwm1Regs.TZFRC.all=0;
 EPwm2Regs.TZFRC.all=0;
 EPwm3Regs.TZFRC.all=0;
 EPwm4Regs.TZFRC.all=0;
 EPwm5Regs.TZFRC.all=0;
 EPwm6Regs.TZFRC.all=0;
    EPwm1Regs.ETSEL.bit.SOCAEN = 1;        // Enable SOC on A group  ADC触发信号
    EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRD;       // Select SOC from PRD
    EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST;        //一个事件触发一次ADC
   
 EPwm2Regs.ETSEL.all=0;
 EPwm3Regs.ETSEL.all=0;
 EPwm4Regs.ETSEL.all=0;
 EPwm5Regs.ETSEL.all=0;
 EPwm6Regs.ETSEL.all=0;
 EPwm1Regs.ETFLG.all=0;
 EPwm2Regs.ETFLG.all=0;
 EPwm3Regs.ETFLG.all=0;
 EPwm4Regs.ETFLG.all=0;
 EPwm5Regs.ETFLG.all=0;
 EPwm6Regs.ETFLG.all=0;
 EPwm1Regs.ETCLR.all=0;
 EPwm2Regs.ETCLR.all=0;
 EPwm3Regs.ETCLR.all=0;
 EPwm4Regs.ETCLR.all=0;
 EPwm5Regs.ETCLR.all=0;
 EPwm6Regs.ETCLR.all=0;
 EPwm1Regs.ETFRC.all=0;
 EPwm2Regs.ETFRC.all=0;
 EPwm3Regs.ETFRC.all=0;
 EPwm4Regs.ETFRC.all=0;
 EPwm5Regs.ETFRC.all=0;
 EPwm6Regs.ETFRC.all=0;
 EPwm1Regs.PCCTL.all=0;
 EPwm2Regs.PCCTL.all=0;
 EPwm3Regs.PCCTL.all=0;
 EPwm4Regs.PCCTL.all=0;
 EPwm5Regs.PCCTL.all=0;
 EPwm6Regs.PCCTL.all=0;
// EPwm1Regs.TBCTL.all=0x0006;   // Enable Timer,0012禁止相位装载->0016相位装载
// EPwm2Regs.TBCTL.all=0x0006;
// EPwm3Regs.TBCTL.all=0x0006;
// EPwm4Regs.TBCTL.all=0x0006;
    EPwm1Regs.TBCTL.bit.CTRMODE=TB_COUNT_UP;//上升计数模式
 EPwm1Regs.TBCTL.bit.PHSEN=TB_DISABLE;//使能相位校正功能
 EPwm1Regs.TBCTL.bit.PRDLD=TB_SHADOW;//使能相位校正功能
 EPwm1Regs.TBCTL.bit.SYNCOSEL=TB_CTR_ZERO;//使能相位校正功能
 EPwm1Regs.TBCTL.bit.HSPCLKDIV=1;//设定TBCLK与SYSCLKOUT的关系
 EPwm1Regs.TBCTL.bit.CLKDIV=0;//设定TBCLK与SYSCLKOUT的关系
 
    EPwm2Regs.TBCTL.bit.CTRMODE=TB_COUNT_UP;//上升计数模式
 EPwm2Regs.TBCTL.bit.PHSEN=TB_DISABLE;//使能相位校正功能
 EPwm2Regs.TBCTL.bit.PRDLD=TB_SHADOW;//使能相位校正功能
 EPwm2Regs.TBCTL.bit.SYNCOSEL=TB_SYNC_IN;//使能相位校正功能
 EPwm2Regs.TBCTL.bit.HSPCLKDIV=1;//设定TBCLK与SYSCLKOUT的关系
 EPwm2Regs.TBCTL.bit.CLKDIV=0;//设定TBCLK与SYSCLKOUT的关系
 
 EPwm3Regs.TBCTL.bit.CTRMODE=TB_COUNT_UP;//上升计数模式
 EPwm3Regs.TBCTL.bit.PHSEN=TB_DISABLE;//使能相位校正功能
 EPwm3Regs.TBCTL.bit.PRDLD=TB_SHADOW;//使能相位校正功能
 EPwm3Regs.TBCTL.bit.SYNCOSEL=TB_SYNC_IN;//使能相位校正功能
 EPwm3Regs.TBCTL.bit.HSPCLKDIV=1;//设定TBCLK与SYSCLKOUT的关系
 EPwm3Regs.TBCTL.bit.CLKDIV=0;//设定TBCLK与SYSCLKOUT的关系
 
 EPwm4Regs.TBCTL.all=0x0006;
 EPwm5Regs.TBCTL.all=0x0006;
 EPwm6Regs.TBCTL.all=0x0006;
 
 EPwm1Regs.TBPRD=SP;
 EPwm2Regs.TBPRD=SP;
 EPwm3Regs.TBPRD=SP;
 EPwm4Regs.TBPRD=SP;
    EPwm5Regs.TBPRD=SP;
    EPwm6Regs.TBPRD=SP;
   
    EPwm1Regs.CMPA.half.CMPA =SP;
 EPwm2Regs.CMPA.half.CMPA =SP;
 EPwm3Regs.CMPA.half.CMPA =SP;
 EPwm4Regs.CMPA.half.CMPA =SP;
 EPwm5Regs.CMPA.half.CMPA =SP;
 EPwm6Regs.CMPA.half.CMPA =SP;
 EPwm4Regs.CMPB=SP;
// EPwm4Regs.CMPB=SP;
// EPwm1Regs.CMPB=SP;
// EPwm2Regs.CMPB=SP;
// EPwm3Regs.CMPB=SP;
// EPwm1Regs.ETCLR.bit.INT=1;
// PieCtrlRegs.PIEACK.all=PIEACK_GROUP3;
#if 0
    EPwm5Regs.TBSTS.all=0;
 EPwm5Regs.TBPHS.half.TBPHS=0;
 EPwm5Regs.TBCTR=0;
 EPwm5Regs.CMPCTL.all=0x50;        // Immediate mode for CMPA and CMPB
 EPwm5Regs.CMPA.half.CMPA =SP*3/4;
 //EPwm1Regs.CMPB=SP/2;
 EPwm5Regs.AQCTLA.all=0x90;        // EPWMxA = 1 when CTR=CMPA and counter inc                                  // EPWMxA = 0 when CTR=CMPA and counter dec
   // EPwm1Regs.AQCTLB.all=0x600;
// EPwm1Regs.AQCTLB.all=0;
 EPwm5Regs.AQSFRC.all=0;
 EPwm5Regs.AQCSFRC.all=0;
 EPwm5Regs.DBCTL.bit.IN_MODE=0;
 EPwm5Regs.DBCTL.bit.OUT_MODE=3;
 EPwm5Regs.DBCTL.bit.POLSEL=2;
 EPwm5Regs.DBFED=300;
 EPwm5Regs.DBRED=300;
 EPwm5Regs.TBCTL.all=0x0010+TBCTLVAL;   // Enable Timer
 EPwm5Regs.TBPRD=SP;
#endif
  • 你好,应该是移相生成的原理造成的,是移相控制特有的。任何的移相PWM都有这个现象无论是数字还是模拟的
  • 你好,这个程序里面没有用到移相控制,就是一个循环改变频率以及占空比的逻辑
  • 供参考
    The following are some general guidelines. There are likely many other choices that one can make for a particular power stage/application that may provide benefits to that particular use case.
    1.Up and down count PWM operations give 2x the number of cycle counts than up-down count operation at the same PWM frequency.a.This means you can achieve higher resolution.



    2.Symmetric (up-down count) PWM methods are often used when low harmonic distortion is desired.
    3.HRPWM (High-Resolution PWM) operation on C2000 devices imposes some duty cycle value restrictions.a.For up or down count modes, without high resolution period: A loss of 3 system clock duty cycle steps in one PWM period.
    b.For up count mode, with high-resolution period: A loss of 6 system clock duty steps.
    c.For up-down count mode, with high-resolution period: A loss of 12 system clock duty cycle steps.

    4.If HRPWM period control is desired, only up-count or up-down count mode may be used. Down-count mode is not supported.
    5.When phase shift between PWMs is the controlled parameter, having PWMs configured in asymmetric mode is typically easier to handle than symmetric mode. This is because when phase shift is greater 180 deg, it necessitates the synchronized PWM to be configured to count in the other direction on a sync event than how it was configured for phase shift < 180 deg. This must be handled by software.
    6.If a constant 50 % duty cycle is desired, it is easier to use up-down count mode and have action qualifier events configured at CTR = 0 and PRD. If high-resolution period control is desired, this action qualifier configuration is not recommended.