This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问AD乒乓采样为什么一直停留在while语句?

Other Parts Discussed in Thread: TMS320F28027

采用下面一段程序。其中EALLOW和EDIS是我加的。发现程序一直停留在while (AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){}或while (AdcRegs.ADCINTFLG.bit.ADCINT2 == 0){;}语句。具体的表现是while( index < SampleSize )只能循环一次,第二次循环就停留在while (AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){}或while (AdcRegs.ADCINTFLG.bit.ADCINT2 == 0){;}。

相应的寄存器的值为:

ADCCTL1 0x4FE4
ADCINTOVF 0x0002
INTSEL1N2 0x2E26
ADCPRICTL 0X01E0
ADCINTSOCSEL1 0xAAAA
ADCINTSOCSEL2 0X5555
ADCSOC0CTRL到ADCSOC15CTL均为0X0006
ADCREFTRIM 0X2979
ADCOFFTRIM 0X01FB

调试时发现在第一个WHILE的时候,当第一次检测到ADCINT1为1的时候,也检测到ADCINT2为1,可能是采用ADCINT1作为第二组的SOC引起的,即第一组的八个AD刚转换好,立即又启动第二组的转换。在第一个循环中ADCINT1和ADCINT2可以正常清0。但while( index < SampleSize )的第二次循环的过程中就不正常了。有时候第一次的ADCINT2不能触发第二次循环的SOC6,有时候第二次循环的ADCINT1不能触发第二次循环的后一组的SOC14。不知是不是软件来不及,因为ADCINTOVF标志不为0。但这个应该不是连续转换。虽然后来循环中也用软件触发可以让软件继续运行,但这段程序为什么第二次循环后就不能将ADCINT1或ADCINT2置为1是什么原因呢?

程序代码:

Uint16 AdcConversion(void)
{
Uint16 index, SampleSize, Mean, ACQPS_Value;
Uint32 Sum;

index = 0; //initialize index to 0
SampleSize = 256; //set sample size to 256 (**NOTE: Sample size must be multiples of 2^x where is an integer >= 4)
Sum = 0; //set sum to 0
Mean = 999; //initialize mean to known value

//Set the ADC sample window to the desired value (Sample window = ACQPS + 1)
ACQPS_Value = 6;
EALLOW;
AdcRegs.ADCSOC0CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC1CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC2CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC3CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC4CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC5CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC6CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC7CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC8CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC9CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC10CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC11CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC12CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC13CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC14CTL.bit.ACQPS = ACQPS_Value;
AdcRegs.ADCSOC15CTL.bit.ACQPS = ACQPS_Value;


//Enable ping-pong sampling

// Enabled ADCINT1 and ADCINT2
AdcRegs.INTSEL1N2.bit.INT1E = 1;
AdcRegs.INTSEL1N2.bit.INT2E = 1;

// Disable continuous sampling for ADCINT1 and ADCINT2
AdcRegs.INTSEL1N2.bit.INT1CONT = 0;
AdcRegs.INTSEL1N2.bit.INT2CONT = 0;

AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINTs trigger at end of conversion

// Setup ADCINT1 and ADCINT2 trigger source
AdcRegs.INTSEL1N2.bit.INT1SEL = 6; //EOC6 triggers ADCINT1
AdcRegs.INTSEL1N2.bit.INT2SEL = 14; //EOC14 triggers ADCINT2

// Setup each SOC's ADCINT trigger source
AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 2; //ADCINT2 starts SOC0-7
AdcRegs.ADCINTSOCSEL1.bit.SOC1 = 2;
AdcRegs.ADCINTSOCSEL1.bit.SOC2 = 2;
AdcRegs.ADCINTSOCSEL1.bit.SOC3 = 2;
AdcRegs.ADCINTSOCSEL1.bit.SOC4 = 2;
AdcRegs.ADCINTSOCSEL1.bit.SOC5 = 2;
AdcRegs.ADCINTSOCSEL1.bit.SOC6 = 2;
AdcRegs.ADCINTSOCSEL1.bit.SOC7 = 2;
AdcRegs.ADCINTSOCSEL2.bit.SOC8 = 1; //ADCINT1 starts SOC8-15
AdcRegs.ADCINTSOCSEL2.bit.SOC9 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC10 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC11 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC12 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC13 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC14 = 1;
AdcRegs.ADCINTSOCSEL2.bit.SOC15 = 1;
EDIS;
DELAY_US(ADC_usDELAY); // Delay before converting ADC channels


//ADC Conversion

AdcRegs.ADCSOCFRC1.all = 0x00FF; // Force Start SOC0-7 to begin ping-pong sampling

while( index < SampleSize ){

//Wait for ADCINT1 to trigger, then add ADCRESULT0-7 registers to sum
while (AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){}
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Must clear ADCINT1 flag since INT1CONT = 0

Sum += AdcResult.ADCRESULT0;
Sum += AdcResult.ADCRESULT1;
Sum += AdcResult.ADCRESULT2;
Sum += AdcResult.ADCRESULT3;
Sum += AdcResult.ADCRESULT4;
Sum += AdcResult.ADCRESULT5;
Sum += AdcResult.ADCRESULT6;
Sum += AdcResult.ADCRESULT7;

//Wait for ADCINT2 to trigger, then add ADCRESULT8-15 registers to sum
while (AdcRegs.ADCINTFLG.bit.ADCINT2 == 0){;}
AdcRegs.ADCINTFLGCLR.bit.ADCINT2 = 1; //Must clear ADCINT2 flag since INT2CONT = 0

Sum += AdcResult.ADCRESULT8;
Sum += AdcResult.ADCRESULT9;
Sum += AdcResult.ADCRESULT10;
Sum += AdcResult.ADCRESULT11;
Sum += AdcResult.ADCRESULT12;
Sum += AdcResult.ADCRESULT13;
Sum += AdcResult.ADCRESULT14;
Sum += AdcResult.ADCRESULT15;

index+=16;

} // end data collection

//Disable ADCINT1 and ADCINT2 to STOP the ping-pong sampling
EALLOW;
AdcRegs.INTSEL1N2.bit.INT1E = 0;
AdcRegs.INTSEL1N2.bit.INT2E = 0;
EDIS;

Mean = Sum / SampleSize; //Calculate average ADC sample value

return Mean; //return the average

}//end AdcConversion