根据下面这个pdf文件利用TI的controlSUITE里面serial_flash_programmer程序进行DSP28377的串口加载,每次加载完F2837xD_sci_flash_kernels_cpu01.txt文件就无法再进行下一步操作了。请问一下大家有遇过类似的情况吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据下面这个pdf文件利用TI的controlSUITE里面serial_flash_programmer程序进行DSP28377的串口加载,每次加载完F2837xD_sci_flash_kernels_cpu01.txt文件就无法再进行下一步操作了。请问一下大家有遇过类似的情况吗?
0==0
0==0
0==0
Bit rate /s of transfer was: 5377.048828
What operation do you want to perform?
1-DFU
2-Erase
3-Verify
4-Unlock Zone 1
5-Unlock Zone 2
6-Run
7-Reset
0-DONE
1
calling f021_SendPacket
Downloading led.txt to device...
您好,在Windows CMD窗口执行完“serial_flash_programmer.exe -d f2837xS -k F2837xD_sci_flash_kernels_cpu01.txt -a led.txt -b 9600 -p COM3” 语句之后
程序执行到这一步之后就不能再往下进行了,按照提示输入“1”之后,程序处于一直等待的状态。
还有就是,有没有方法不用下载kernel文件,直接下载程序,实现sci加载呢?