This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

park,ipark变换的Angle要不要标幺呢?谢谢



您好!

1.做三相整流器,软件锁相出来的Angle为0到2*PI的范围,同时送给park,ipark做变换用,请问要不要标幺化呢?park,ipark中的Angle有没有范围要求呢?谢谢!

 

2.额,多问下,是不是dsp中所有的计算都要用标幺值呢,比如锁相用的表达式Angle=Angle+2*pi*50(W),假如是这样的表达式,其中的角频率W=2*pi*50要不要标幺化写为1计算呢(其中角频率基值为2*pi*f,f为额定电网频率)?

再次感谢!

  • 角度Angle应该是要标幺化的,范围是-1~1,采用Q格式表示(具体Q几根据用户程序约定)。

    在我了解中,电机控制方面的程序中基本都采用标幺值表示和计算。谢谢!

  • 角度的范围可以是0到2PI,也可以归一化到0到1,取决于三角函数如何计算。

    在TI的例程中,角度是归一化的,其范围是0~1,Q格式表示(00000000-7FFFFFFF)。

    在实际使用中,角度的归一化计算也很简单。比如,采用光编作为传感器,如果是2000线的光编,那么读到的编码器值除以2000就得到了归一化后的机械角度值。