This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28379d EPWM 变TBPRD变频 发现输出pwm信号在一段时间内被拉低或者拉高



采用controlCard tms32028379d来实现EPWM变频输出,系统时钟200MHz, EPWM时钟100MHz.  相关代码如下:

if((fabs(EPwm2Regs.TBPRD - CRM_Ctrl.BPRD) < 40)&&(CRM_Ctrl.BPRD >= 99)&&(CRM_Ctrl.BPRD <= 500)&&(EPwm2Regs.TBPRD < CRM_Ctrl.BPRD))
{

Frequency_change_cnt++;

EALLOW;

GpioDataRegs.GPATOGGLE.bit.GPIO12 = 1;
EPwm2Regs.TBPRD = CRM_Ctrl.BPRD;
PI_TLBDC_I[0].d_s1 = CRM_Ctrl.New_Dton;

EDIS;

}

通过改变PWM2模块中寄存器EPwm2Regs.TBPRD来实现变频,发现在写TBPRD的时候,输出PWM2信号在一段时间内会被拉低或者拉高,持续时间在1ms左右,之后又恢复正常,变频范围在500kHz~1MHz, 尝试改变TBCTL.PRDLD发现问题依然存在。

PWM相关寄存器配置如下:

 

EPwm2Regs.TBPRD =199; //PWM period
EPwm2Regs.TBPHS.bit.TBPHS = 0;//TLBDC_PHASE(120.0f);//0; //No phase shift
EPwm2Regs.TBCTL.bit.FREE_SOFT = 2; //Free run
// EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP; //Counter up after synchronization
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; //System clock out / 1
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; //System clock out / 1
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;//TB_CTR_ZERO;//TB_SYNC_IN;//TB_CTR_ZERO; //Send synchronization signal when counter = 0
EPwm2Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;//TB_SHADOW; //Using shadow register for PWM period
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;//TB_DISABLE;//TB_DISABLE; //Master, don't need load phase register
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;//TB_COUNT_UPDOWN; //TB_COUNT_UP;//Up-down mode

EPwm2Regs.CMPA.bit.CMPA = 0;//TLBDC_CMPA(0.3);//cmpa=zkb*prd(s1),zkb=pi_out
EPwm2Regs.CMPB.bit.CMPB = 0;//TLBDC_CMPB(0.3);//phase=180; zkb'=pi_out,cmpb=(1-zkb')*prd=(1-pi_out)*prd (s2,pass a not logic->s3)
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;//CC_SHADOW;//Using shadow register for compare
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;//CC_SHADOW;//Using shadow register for compare
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;//Load new compare value when counter = period
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;//CC_CTR_ZERO;//Load new compare value when counter = zero

EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR;//AQ_SET; // Set PWM1A on Zero
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; //AQ_CLEAR; // Clear PWM1A on event A,
// up count
EPwm2Regs.AQCTLB.bit.ZRO = AQ_SET; // Set PWM1B on Zero
EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Clear PWM1B on event B,

EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;//DBA_RED_DBB_FED;//DBB_RED_DBA_FED;//s5=1,s4=0
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;//DBB_ENABLE;//DB_DISABLE;//DBB_ENABLE;// s1=0,s0=1(Q3)->0(Q2)
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;//DB_ACTV_LOC;//DB_ACTV_HI;//DB_ACTV_LO;//0x00;//DB_ACTV_HIC;// s3=1,s2=0->1, Active Hi complementary
EPwm2Regs.DBFED = 0x05;//INV_DEAD_CYCLE;// FED = INV_DEAD_CYCLE TBCLKs
EPwm2Regs.DBRED = 0x02;//INV_DEAD_CYCLE;// RED = INV_DEAD_CYCLE TBCLKs
EPwm2Regs.DBCTL.bit.OUTSWAP = 0x00;//0x03;

//add soca
EPwm2Regs.ETSEL.bit.SOCAEN=ET_ENABLE;//enable
EPwm2Regs.ETSEL.bit.SOCASEL=ET_CTR_PRDZERO;//ET_CTR_PRDZERO;
EPwm2Regs.ETPS.bit.SOCAPRD=ET_1ST;//divide frequency, page69/117.



EPwm2Regs.ETSEL.bit.SOCBEN=ET_ENABLE;//enable
EPwm2Regs.ETSEL.bit.SOCBSEL=ET_CTR_PRDZERO;//ET_CTR_ZERO;
EPwm2Regs.ETPS.bit.SOCBPRD=ET_1ST;//divide frequency

EPwm2Regs.ETSEL.bit.INTEN=ET_DISABLE;
EPwm2Regs.ETPS.bit.INTPRD=ET_DISABLE;

EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_TZ1; // DCAH = TZ1

EPwm2Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI;//TZ_DCAH_LOW;//TZ_DCAL_HI_DCAH_LOW;

EPwm2Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT1; //DCAEVT1 =DCAEVT1(not filtered)
EPwm2Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC;//DC_EVT_SYNC;//DC_EVT_ASYNC;//DC_EVT_SYNC;// // Take async path

EPwm2Regs.TZCTL.bit.TZA = TZ_NO_CHANGE;//TZ_FORCE_HI; // EPWM1A will go high
EPwm2Regs.TZCTL.bit.TZB = TZ_NO_CHANGE;//TZ_FORCE_LO; // EPWM1B will go low

EPwm2Regs.TZCTL.bit.DCAEVT1 = TZ_NO_CHANGE;//TZ_FORCE_HI; // EPWM1A will go high

EPwm2Regs.DCACTL.bit.EVT1SYNCE = 1;

 

1.是有什么寄存器没有配置正确导致的吗,比如shadow register或者AQ之类的导致在写TBPRD的时候会被强制拉低或者拉高?

2.TI有没有相关的变频的例程啊 我找了很久都没找到?

 

  • 你好,你设计的频率变化范围是多少?如果设置变化范围小一点还会有这种情况吗?例如从1MHz变为950kHz。
    例程的话目前确实还没开发这类例程。
  • 如果是周期出现的 可能是寄存器等没有配置好 如果是偶尔出现的 建议你将输出管脚之后的负载去掉
    只接示波器看看是否还出现这个问题
  • 变频范围在500kHz~1MHz,每次切换的频率不会太大,软件上有限制的

    我定频跑500kHz和1MHz都没有问题


    此外我发现当我连接XDS100V2 USB 仿真器跑的时候会有一个100kHz的干扰,就是每隔100kHz 时duty就会变大或者变小,其余时刻都正常,当我把程序烧录到Flash 之后跑就没有问题了,请问我这个100kHz是仿真器产生的吗?