This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用28375D,双核调试。CPU1进入ILLEGAL_ISR中断。



双核在线调试。

如果只烧写CPU1全速运行一切正常。

如果烧写了CPU1,CPU2。CPU1直接运行进入ILLEGAL_ISR中断。

如果烧写了CPU1,CPU2。CPU2先运行,在运行CPU1,也进入ILLEGAL_ISR中断。

CPU1进入ILLEGAL_ISR中断后,重启(Restart),CPU1可以正常运行但是CPU1进不来中断程序。

CPU1的CMD
MEMORY
{
PAGE 0 : /* Program Memory *///PAGE0是程序空间
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE //CPU自用内存 M0~Mx
RAMD0 : origin = 0x00B000, length = 0x000800 //CPU自用内存 D0~Dx
RAMLS0 : origin = 0x008000, length = 0x002200 //LS,CPU及其自身CLA公用内存
//RAMLS1 : origin = 0x008800, length = 0x000800
//RAMLS2 : origin = 0x009000, length = 0x000800
//RAMLS3 : origin = 0x009800, length = 0x000800
//RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x003FFE /* on-chip Flash */
//FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHB : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHDE : origin = 0x086000, length = 0x018000 /* on-chip Flash */
//FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
//FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
//FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 : /* Data Memory *///数据空间
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800

RAMLS5 : origin = 0x00A800, length = 0x000800

RAMGS0 : origin = 0x00C000, length = 0x001000 //子系统CPU和DMA之间共享 GS0~GSx
RAMGS1 : origin = 0x00D000, length = 0x004000
// RAMGS2 : origin = 0x00E000, length = 0x001000
// RAMGS3 : origin = 0x00F000, length = 0x001000
// RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000


CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}


SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHDE PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)

MainLoop : LOAD = FLASHDE,
RUN = RAMLS0 ,
LOAD_START(_MainLoopLoadStart),
LOAD_SIZE(_MainLoopLoadSize),
LOAD_END(_MainLoopLoadEnd),
RUN_START(_MainLoopRunStart),
RUN_SIZE(_MainLoopRunSize),
RUN_END(_MainLoopRunEnd),
PAGE = 0, ALIGN(4)

#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHDE,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHDE,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif

/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1

/* Initalized sections go in Flash */
.econst : >> FLASHH PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)

.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}

GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

CPU2的CMD


MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000080, length = 0x000380
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS15 : origin = 0x01B000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 :

BOOT_RSVD : origin = 0x000002, length = 0x00007E /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800

RAMLS5 : origin = 0x00A800, length = 0x000800


CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}

SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : > FLASHB PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)

/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAMLS5 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1

/* Initalized sections go in Flash */
.econst : > FLASHB PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif

/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}

GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/