This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问28377D的Upp模块支持与FPGA的半双工通信吗?



第一次接触Upp,想要利用Upp模块实现DSP与FPGA的通信,功能如下:

1. 利用Upp从FPGA收取所需数据,DSP处理后将数据返回给FPGA;

2. 已编写Verilog程序并调试,FPGA程序运行正常;

3. Upp模块只收或者只发,完全正确;

4. 先设置Upp工作与Receive,收取数据后,重配置寄存器工作与Transfer模式,结果完全混乱。

所以,想问一下28377D的Upp模块是否无法工作于半双工模式下?如果可以,该如何设置,谢谢!

另外,想问一下28377D的DMA占用了地址0x7000,但是在RAM memory Map中,0x7000并没有分配给Upp DMA,而是给了WatchDog,想问一下这是怎么回事?谢谢。

  • 你好,不支持双工模式,只支持单工模式:
    The uPP interface is a high-speed parallel interface with dedicated data lines and minimal control signals.
    The uPP interface is designed to interface cleanly with high-speed ADCs or DACs with 8-bit data width. It
    can also be interconnected with field-programmable gate arrays (FPGAs) or other uPP devices to achieve
    high-speed digital data transfer. It can operate in receive mode or transmit mode (simplex mode).
  • 谢谢,解答了我的问题!