错误联防(TZ)子模块可以工作在OSHT模式和CBC模式
Reference Guide中描述
OSHT是作为主短路和过流的情况,
CBC是作为电流限定。
OSHT模式工作在短路和过流的情况下,可以理解,可直接将EPWMXA/EPWMXB设置成设定状态。
但是CBC 是怎么限流的呢?
求解!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先这里说的限流是针对采用PWM信号控制开关器件的功率回路来说的。
电流反馈信号,接到外置或片内比较器上,比较器输出接TZ的输入。
If the cycle-by-cycle trip
event is still present when the CBC bit is cleared, then CBC will be immediately set again. The
specified condition on the pins is automatically cleared when the ePWM time-base counter
reaches zero (TBCTR = 0x0000) if the trip condition is no longer present. The condition on the
pins is only cleared when the TBCTR = 0x0000 no matter where in the cycle the CBC flag is
cleared.
这一段是在ti的pdf里找到的,请问这里的pins是什么意思啊? 是不是要先设置pins脚的功能,由这个pins而引发事件啊?谢谢!