This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

多块28062从机 MCBSP MDX脚连接问题



多个28062当从机时,从机的MDX脚能直接并联连起来,还是要通过与门再输出到主机上。

当存在多个28062当从机时,MCBSP开启了通道选择,在一帧中,一个从机的发送通道已经到来,另一个从机的发送通道还没有到来,那么通道还未到来的从机MDX管教是处以高阻抗状态呢还是高电平状态,如果是高电平状态,当通道已经到来的从机MDX脚输出低电平,会不会存在大电流从通道还没有到来的从机流向通道已经到来的从机。

  • MDX作为发送数据 也就是发送端只能有一个 可以有多个从端 如果驱动能力不够可以增加驱动芯片
    如果发送有多个 就会出现竞争现象
  • Q: How will all the slaves send to the data to the master at the same time?

    A:This is not possible using the McBSP. If TDM is used, each slave will have a time slot on the bus to transmit data, but the master cannot accept data from multiple slaves all at the same time. If TDM is not an approach you want to choose, you can also use the McBSP in SPI mode with multiple GPIOs as custom chip selects. Before the master sends data, it will set all slaves active by setting their chip selects low, transmit data, then make all slaves inactive by setting the chip select high. The master must control every transmission, so to read data back from a slave, the master should only enable one slave at a time to receive data. Look at multi-slave SPI protocols to see how this approach might work.

    主设备每次只能启用一个从设备来接收数据,也就是从机发送端每次只能有一个
  • 默认的从机接收端应该是只有一个
  • 从机的发送时钟和帧同步信号,也是主机产生的,主从机都启用了TDM通道选择,举个例子,主机时钟产生模块,为64个字产生一次帧同步信号,主机发送0~55通道,接受0~55通道,帧长为56字,从机1发送0~31通道,接受0~31通道,帧长32字,从机2发送32~55通道,接受32~55通道,帧长32字,所以时序上是不存在竞争,但是我想知道从机在非自己通道的时候,MDX管教状态是高阻抗还是就是高电平。