This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

drv8353rh_evm开发板 3.3VLDO发热问题

Other Parts Discussed in Thread: LP2992

板卡上的稳压管 型号 LP2992IM5-3.3/NOPB,12V的输入 提供3.3V输出,250mA的固定输出,插上 控制板卡ISO-F28027F 发热现象严重 ,(没有测温设备)手无法长时间触碰的情况,拔掉控制板ISO-F28027F给驱动板单独上电,是24V 3mA的功耗 ; 控制板卡ISO-F28027F单独上电是 3.3V 58mA的功耗; 相当于200mA的电流发热耗掉了,这个现象正常吗,长时间使用会有问题吗?

  • 对LP2992芯片不是很熟悉,根据datasheet,芯片工作电流最大是80mA。如果确实电源芯片输出固定250mA的话,长期使用肯定是不推荐的,去掉芯片外围电路的消耗,也会给芯片带来压力。另外,芯片正常在-40~125度都能工作,一般工作的时候在40~80度也比较正常。建议测试一下具体多少温度。
  • 这个确实不好说 如果插到一起功能都跑起来 这个功耗也是合理的
    建议你在确保温度范围内后进行功能验证是否合理