This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运行28377的cla_adc_fir32_cpu01例程时cla任务程序未运行



如题,在运行例程时发现cla并未运行,通过查阅网络资料,初步推断是并未将cla从flash中导入ram所致。在CLA_configClaMemory中找到memcpy((uint32_t *)&Cla1funcsRunStart, (uint32_t *)&Cla1funcsLoadStart,(uint32_t)&Cla1funcsLoadSize);但是并未编译,进行编译后报错unresolved symbol _Cla1funcsRunStart,first referenced in./cla_adc_fir32_cpu01.obj以此类推语句中三个变量都报了这种故障。但是在CLA_configClaMemory中进行了extern uint32_t Cla1funcsRunStart, Cla1funcsLoadStart, Cla1funcsLoadSize;声明。

想请问想运行cla该怎么办???