Other Parts Discussed in Thread: TLV803
2个批次F28335电路板,所有电路图,贴片芯片型号完全一致;
第一个批次上电均能正常工作;第二个批次电路板部分F28335无法进入主程序;
已设计为1.9V电源先启动,3.3V后启动,RC上电复位(10ms),30M有源晶振;(1.9V电源输出接到3.3V电源使能端,开关电源芯片,纹波<50mV)
针对部分无法正常工作的F28335,测量电路板:
1、3.3V 1.9V电源正常,加大或减小3.3V和1.9V电容无效
2、晶振已经起振,更换晶振无效
3、怀疑F28335未焊接好,重新拖锡焊接无效
4、怀疑RC及二极管复位电路问题,更换RC,二极管,换大或换小RC时间常数无效,1ms-1s均试过
5、怀疑RC复位不行,更换TLV803上电复位芯片,上电时仍出现无法进入主程序情况,但是在5-6s后MCU正常进入主程序;正常<1s
6、出现无法进入主程序的电路板,断电后5-6s内再次上电,运行正常,立刻进入主程序;若断电时间>10s以上,必然再次出现无法进入主程序;
电路板断电后1s内所有电容的电立刻会被消耗掉,没有任何电池
以上为故障描述,请教大神!!