条件:已配置好1ms定时中断A。
需求:定时中断A每间隔10次中断后,在中断A中软件触发产生一次用户中断B。(即10ms产生一次中断B)
在用户中断B中每间隔10次中断后,软件触发产生一次用户中断C。(即100ms产生一次中断B)
中断优先级为A>B>C。
B的任务执行时间大于1ms,小于10ms,所以需要A打断B的需求。B和C同理
问题:如何配置B和C 中断,B和C可以采用什么中断?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.